STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RTC Wakeup interrupt not triggering on STM32L100

Posted on November 17, 2015 at 15:09Hello,It seems that the IRQ handler for the wakeup does not trigger even the RTC is running correctly, WUTIE is set in CR register and the ISR flag WUTF is set as expected. What could be the issue? The FW is build...

juho by Associate II
  • 1767 Views
  • 2 replies
  • 0 kudos

STM32F4-Discovery Boot0/1 De-soldering

Posted on November 17, 2015 at 23:37Greetings,I'm wanting to shave every bit of power I can off of this board and was thinking of de-soldering the Boot0 and Boot1 bridges.  Question is, will this adversely effect the bootloader in any way?  Currentl...

shawn2 by Associate II
  • 729 Views
  • 0 replies
  • 0 kudos

STM32F4 Timer External Pulse counting

Posted on May 18, 2013 at 00:23Since 4 day I'm trying write code which will be able to count external pulses. I tried to use encoder mode but i supposed that this work only with 2 quadrature encoders. I have only one pulse signal and i have no idea ...

STM32f4 discovery board

Posted on November 16, 2015 at 17:27Hello,I have a problem with running a  TFT. My LCD chip is SSD1289 . I have communication between the board ( stm32f407 - discovery ) and the LCD but there isn't a text on the screen. I attach my code.

STM32F0 DMA communication

Posted on November 16, 2015 at 16:22 Hi all,i want to STM32F0 DMA communication Peripheral to Perpheral.but when i debugging my codes,in my while loop code works one time and stops.What is my fault.My code is here; /* Includes -----------...

STM32F and USB at 1.8V

Posted on November 16, 2015 at 18:54I would like to connect an STM32F405 to usb while running the chip at 1.8V. Since USB requires 3.3V I need some kind of level translator. I have tried the TSX0102 and did not get it working. Has anyone done this b...

sburr by Associate II
  • 2109 Views
  • 3 replies
  • 0 kudos

Bulk data transfer on CAN bus

Posted on November 13, 2015 at 22:40 Hi guys i have managed to communicate using CAN protocol now i want to send around 200 16 bit values from 1 stm32f4 to another stm32f4 below is the code to transfer 8 values, How can i improve my code to tran...

puneethj by Associate II
  • 5566 Views
  • 7 replies
  • 0 kudos

SWD debugging problem

Posted on November 17, 2015 at 12:34i made my stm32f030k6t6 board and i connect it to stlink after that  i generate keil V5 project using stmcube .i  enabled the SWD pins only , after that i compiled the program and download it ,i start the debugger...

0690X00000605JqQAI.png
eng239955 by Associate II
  • 2569 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.