STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 USB disable endpoint interrupt is not generated

Posted on August 17, 2014 at 23:13I'm working on usb device project and I need after receiving a command from the host to return the device to predetermined state. To do this, all prepared OUT transfers must be canceled. I set endpoint disable bit(E...

SD High Speed Switching

Posted on November 18, 2015 at 15:20Hi, do anybody know how to switch SD operation from Default mode to High Speed Mode in WICED using SD_CMD_HS_SWITCH command??I have added    SDIO_CmdInitStructure.SDIO_Argument = 0x80FFFF01;    SDIO_CmdInitStructu...

abhijith by Associate
  • 1048 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F407VG Timers Synchronization question.

Posted on November 13, 2015 at 18:42Hello everyone, i need some help, so if anyone could, i'd be grateful. I need to start two timers instantaneously at the same time, when external event happens. Lets say, rising edge on the pin should trigger two ...

RTC Wakeup: HAL_RTCEx_SetWakeUpTimer_IT

Posted on November 18, 2015 at 16:51I resolved my problem, I had to enable the interrupt into the NVIC, before activating the WKUP_IT:    /* Enable and set RTC_WKUP_IRQ */    HAL_NVIC_SetPriority(RTC_WKUP_IRQn, 2, 0);    HAL_NVIC_EnableIRQ(RTC_WKUP_...

cyril by Associate II
  • 1276 Views
  • 1 replies
  • 0 kudos

Missing BlueNRG driver for NUCLEO-F103RB?

Posted on November 17, 2015 at 11:18Dear all,I have a NUCLEO-F103RB together with a X-NUCLEO-IDB04A1 Bluetooth extension board.Now I wanted to start learning how to program with bluetooth and downloaded x-cube-ble1.zip from STM website.Inside the fo...

timon by Associate
  • 877 Views
  • 1 replies
  • 0 kudos

STM32F030R8 TIM3 remap to port C

Posted on November 17, 2015 at 09:58Hi guys I referred to the timer 3 channels remapped to port C for STM32F030R8. The datasheet DM00088500 version 2 page 30 did not mention there is a restriction for the mapping, while page 37 do carry a small (1) ...

V CORE domain clocks

Posted on November 17, 2015 at 18:55In document DM00108282.pdf(RM0377) page 143 it mentions V CORE domain clocks. What clocks are included in V Core domain? What clocks are included in Vdd domain?

bigbird by Associate
  • 1214 Views
  • 1 replies
  • 0 kudos

stm32f401re nucleo: USART programming

Posted on November 16, 2015 at 11:38Hello everybody,I'm new on the forum and on ST microcontrollers.I'm trying to program the USART in assembly, but I have some issue to write on DR.What am I missing? Somebody can help me, please?*******************...

life758 by Associate II
  • 2025 Views
  • 6 replies
  • 0 kudos

STM32 stop mode and UART interrupt

Posted on November 18, 2015 at 08:18Hi 1. Can a UART receive interrupt wake the STM32 MCU from Stop mode (RX line start bit) ? 2. Only a External Interrupt can wake the STM32 MCU from low power modes ? Regards #!stm32f4-disco #low-power-stop-mode

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.