2015-11-09 3:26 PM
Disclose any of insiders as it will integrate STM32Cube and new HAL Drivers to the Keil MDK-ARM and his Software pack for STM32Fx?Recently released sw pack STM32F1xxDPF v 2.0.0 for MDK-ARM building on Standard Peripheral lib v3.5.0 and CMSIS OS RTX .STM32CubeMX include new HAL_Driver and FreeRTOS. Thanks to this ''papal schism'' is difficult for exaple use in project generated witch STM32Cube any sw component from MDK Middleware. Whereas a year ago it spoke about closer integration STM32Cube into sw packt for MDK-ARM.May I ask what is planned in this field and when?
See last section in2015-11-09 4:43 PM
Words. Many words. Some of them I even recognize. Communication of a coherent idea? Not so much.
Was this a google translation from another language? Perhaps you could post your question in the original language and a native speaker could answer you.2015-11-17 10:01 AM
OK
One should not
go into
philosophical
debates
in
language
that can not
well
.My English
is very poor
.Plus
I have
typos
in the text
, with / wichSimplify
query
. In yar 2014 I read At the same time, we plan to integrate STM32CubeMX and Keil MDK such that the code generated by STM32CubeMX will be used to configure the drivers. This will greatly simplify device and driver configuration and provide more robust configurations and drivers.See
the last
http://www.keil.com/appnotes/files/apnt_266.pdf
Now isthe end of the year
2015 and last Software pack for MDK-ARM 5.17, for example v2.0.0 STM32F1 use old STM32F10x Standard Peripherals Library v 3.5.0. STMCube32 use new HAL driver for examéle STM32F1 v1,2I do not know
,
for me it
is not
much
integration
, for me it is Papal schism!I'm interested in
further
development
?
He plans to
move to
the new HAL (CubeMX
)of the library
in the
software
pack
for
MDK
-
ARM
?2015-11-17 10:18 AM
May be you're in the wrong church? These questions about when Keil might do things would be better addressed to Keil, no?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.