2015-11-13 1:40 PM
Hi guys i have managed to communicate using CAN protocol now i want to send around 200 16 bit values from 1 stm32f4 to another stm32f4 below is the code to transfer 8 values, How can i improve my code to transfer 200 values.. can i use same STDID
void CAN_Txvalues(void) {
CanTxMsg TxMessage;
// transmit */
TxMessage.StdId = 0x150;
TxMessage.ExtId = 0x00;
TxMessage.RTR = CAN_RTR_DATA;
TxMessage.IDE = CAN_ID_STD;
TxMessage.DLC = 8;
TxMessage.Data[0] = (ADCDmaValuesc1[0] >> 8) ;
TxMessage.Data[1] = (ADCDmaValuesc1[0]);
TxMessage.Data[2] = (ADCDmaValuesc1[1] >> 8) ;
TxMessage.Data[3] = (ADCDmaValuesc1[1]);
TxMessage.Data[4] = (ADCDmaValuesc1[2] >> 8) ;
TxMessage.Data[5] = (ADCDmaValuesc1[2]);
TxMessage.Data[6] = (ADCDmaValuesc1[3] >> 8) ;
TxMessage.Data[7] = (ADCDmaValuesc1[3]);
uint8_t TransmitMailbox = 0;
do
{
TransmitMailbox = CAN_Transmit( CAN2, &TxMessage );
}
while( TransmitMailbox == CAN_NO_MB );
CAN_Txvalues2();// next values
}
void CAN_Txvalues2(void) {
CanTxMsg TxMessage;
// STM_EVAL_LEDOn(LED5);
// transmit */
TxMessage.StdId = 0x151;
TxMessage.ExtId = 0x00;
TxMessage.RTR = CAN_RTR_DATA;
TxMessage.IDE = CAN_ID_STD;
TxMessage.DLC = 8;
TxMessage.Data[0] = (ADCDmaValuesc1[4] >> 8) ;
TxMessage.Data[1] = (ADCDmaValuesc1[4]);
TxMessage.Data[2] = (ADCDmaValuesc1[5] >> 8) ;
TxMessage.Data[3] = (ADCDmaValuesc1[5]);
TxMessage.Data[4] = (ADCDmaValuesc1[6] >> 8) ;
TxMessage.Data[5] = (ADCDmaValuesc1[6]);
TxMessage.Data[6] = (ADCDmaValuesc1[7] >> 8) ;
TxMessage.Data[7] = (ADCDmaValuesc1[7]);
uint8_t TransmitMailbox = 0;
do
{
TransmitMailbox = CAN_Transmit( CAN2, &TxMessage );
}
while( TransmitMailbox == CAN_NO_MB );
}
void CANrx(void) {
if(stdid =150)
{
save data in adc values 0 to 3
}
if(stdid = 151)
{
save data in adc values 4 to 7
}
}
But i badly need to improve the way my code works.. Any help is most welcome
Thanks guys
#becan #!stm32f4-disco
2015-11-13 1:57 PM
But i badly need to improve the way my code works..
Consider using one subroutine, and passing in a pointer, and a message number. And then call that in a loop. Hard coding everything seems like a very bad habit that you need to break as so as possible.2015-11-15 6:20 PM
Assuming you are not using any particular CAN protocol and you don't want to change the message ID then a common method is to use the first two bytes of the data area as the index for the first of three values being sent, followed by three sequential values. For example, the first message would be: 0x0000 val0 val1 val2. This would be followed by: 0x0003 val3 val4 val5, and so on. You can ack each message by sending back just the index.
A more sophisticated method is the SDO transfer used in the CANopen protocol. This uses variations on the above to send variable types and lengths of data. Jack Peacock2015-11-16 3:31 AM
Hey jack, thanks for replying, could you please post an example for SDO transfer, i would like to try that. Thanks
2015-11-16 4:45 AM
SDO (System Data Objects) is part of the open source CANopen network protocol. Search for the CAN in Automation website and you'll find the specifications for it. There are some open source CANopen examples, search for CANfestival.
You need quite a bit of infrastructure to use SDO. It requires a system object dictionary to obtain object metadata (the type and size for an object). In simple terms you send an object ID and the data (in segments if over 32 bit). Jack Peacock2015-11-17 9:18 AM
Hi everyone I read CAN1 has connection to 512 byte SRAM memory so is there any way to save the received frames in the SRAM , if so how to access those messages, if any one already worked on CAN1 with SRAM please help me thank you.
2015-11-17 9:52 AM
I suspect it's used for the Filter/FIFO arrangement. Suggest you review the documentation and look at if/where it is mapped into the 32-bit address range. If it is there, then presumably you can access it like any other memory.
2015-11-17 9:59 AM
That's internal memory, no direct access. Most of the memory is used for filters and FIFOs anyway. Short answer, no you can't use the memory for anything. Incoming messages have to be moved from the two FIFOs (3 deep) and saved somewhere in SRAM. Same for TX, messages have to be queued into one of the three mailboxes.
The memory is only accessible from CAN1 through setting the filters. CAN2 uses the same filter area as CAN1, but a register specifies where the CAN2 filters start. I suppose you could store data in unused filter slots but it would be slow and clumsy, and only save a few bytes of RAM at a cost of many more bytes of flash. Jack PeacockWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.