STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to fire RTC alarm every 1s?

Today, for the first time I tried to set up RTC alarm using STM32U5G9 MCU. I need RTC alarm (IRQ) to fire on every second change, that is, when subsecond counter is zero - it is configured to count 32kHz clock pulses from 32k to 0 using 15-bit subsec...

TDJ_3-1735904047337.png TDJ_1-1735902305185.png TDJ_2-1735902389946.png
TDJ by Lead
  • 2848 Views
  • 2 replies
  • 1 kudos

Resolved! USB CDC dont work in debug

Posted on April 11, 2017 at 12:39Hi all I'm working on a STM32F303CC very simple board(just µC IMU and USB). I need to use a USB Virtual COM (CDC) for a MtoM data transfer with a Windows PC I set up BSP with STMCubeMx and compiling/debuging with Ke...

o gaste by Associate III
  • 6152 Views
  • 4 replies
  • 3 kudos

Resolved! Enable LTDC in CUBEMX

Hi, We are in the designing phase of a STM32H7 board which will control a RGB24 display. To check which package would suit are needs the best we would like to see the RGB pinout on different MCU's. But for some reason I don't find the LTDC interface ...

leddel32 by Associate II
  • 2110 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H563ZIT6 LDO or SMPS?

Hi,does the STM32H563ZIT6 have an LDO and/or an SMPS? Contrary to other micros, I cannot find any table or details about it other than the block diagram common to the whole family (screenshot below) and it says "LDO and/or SMPS". Where on the datashe...

Ricko_0-1735833059659.png Ricko_1-1735833567941.png
Ricko by Senior III
  • 1477 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.