STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Debugger's "Step Over" acts incorrectly

Hi,I am just starting to learn the STMCubeIDE debugger's capabilities. I have tested all the essential functions of the debugger on a led blink project, and after everything worked fine I moved on to an I2C code that actually requires some debugging....

Vilius by Associate III
  • 2259 Views
  • 3 replies
  • 0 kudos

Resolved! Driver STSW-link009 2.0.2 download problem

Hello, I can't download the usb driver STSW-link009 2.0.2 on the "st.com -> development tools"https://www.st.com/en/development-tools/stsw-link009.html#get-softwareWhen I click on "Get latest", I read the licence agreement and click to "Accept"."Get ...

Izitop by Associate II
  • 2071 Views
  • 2 replies
  • 0 kudos

Resolved! Timer output influenced by other timer

Hi everybody,I have TIM15, configured to PWM generation, in one shot configuration, using OC1N output. The output is set to 0 and timer disabled.. When I later initialize TIM1, the output of TIM15 goes high at the instant the Update event is generate...

Resolved! M95P32 EEPROM using QSPI interface on Nucleo-L496ZGP

Board added to title; STM32L4 Label added.I started Working With M95P32 EEPROM which Supports QSPI . This is my code which is not working I don't understand why there is no error in transmit and receive code. But same EEPROM working with SPI.   void ...

Resolved! STM32F207ZG and STM32F407ZG compatibility

Hello everyone,I am currently using the STM32F207ZG in my project, but I am considering replacing it with STM32F407ZG due to speed.After reviewing the two MCUs, I found that the cores and memories of the two MCUs are different, but the peripherals ar...

rndkd1 by Associate II
  • 2114 Views
  • 4 replies
  • 6 kudos

Resolved! How to set the clock source for TIM3

How to set the clock source for TIM3 We are trying to use TIM3. We also want to use an external CLK as the clock source for TIM3, but we don't know how to set it. .ioc file - Where should I change the TIM3 clock source settings?

stm32g474met3 keeps burning out for unknown reason

i have MCU circuit with stm32g474met3 as the processor, designed such that it controls the main board charging circuit and it keeps burning randomly at random times could be 5 hours or 20 minuts or even few days I cant figure out why, it burns whethe...

Untitled design (1).png
Tom12 by Associate II
  • 2455 Views
  • 7 replies
  • 0 kudos

STM32l476 boot inquiry

Hello,The STM32L476 MCU is not booting, and it seems to be stuck at address 0x08000228, as shown in the attached image. It used to boot and work correctly before.At some point, it stopped booting and no longer functions as expected. What could be the...

ksd4692 by Associate II
  • 2204 Views
  • 6 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.