2025-01-06 4:11 AM - last edited on 2025-01-06 8:51 AM by Andrew Neil
Board added to title; STM32L4 Label added.
I started Working With M95P32 EEPROM which Supports QSPI . This is my code which is not working I don't understand why there is no error in transmit and receive code. But same EEPROM working with SPI.
void QSPI_WriteEnable(void) {
QSPI_CommandTypeDef sCommand;
sCommand.InstructionMode = QSPI_INSTRUCTION_1_LINE;
sCommand.Instruction = WRITE_ENABLE_CMD;
sCommand.AddressMode = QSPI_ADDRESS_NONE;
sCommand.DataMode = QSPI_DATA_NONE;
sCommand.DummyCycles = 0;
sCommand.NbData = 0;
sCommand.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, GPIO_PIN_RESET);
HAL_QSPI_Command(&hqspi, &sCommand, HAL_QSPI_TIMEOUT_DEFAULT_VALUE);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, GPIO_PIN_SET);
}
void QSPI_ChipErase(void) {
QSPI_CommandTypeDef sCommand;
sCommand.InstructionMode = QSPI_INSTRUCTION_1_LINE;
sCommand.Instruction = CHIP_ERASE_CMD;
sCommand.AddressMode = QSPI_ADDRESS_NONE;
sCommand.DataMode = QSPI_DATA_NONE;
sCommand.DummyCycles = 0;
sCommand.NbData = 0;
sCommand.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, GPIO_PIN_RESET);
HAL_QSPI_Command(&hqspi, &sCommand, HAL_QSPI_TIMEOUT_DEFAULT_VALUE);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, GPIO_PIN_SET);
}
void QSPI_Write(uint32_t address, uint8_t *data, uint32_t size) {
QSPI_CommandTypeDef sCommand;
QSPI_WriteEnable(); // Enable write
sCommand.InstructionMode = QSPI_INSTRUCTION_1_LINE;
sCommand.Instruction = PAGE_PROGRAM_CMD;
sCommand.AddressMode = QSPI_ADDRESS_1_LINE;
sCommand.Address = address;
sCommand.DataMode = QSPI_DATA_4_LINES;
sCommand.NbData = 1;
sCommand.DummyCycles = 0;
sCommand.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, GPIO_PIN_RESET);
HAL_QSPI_Command(&hqspi, &sCommand, HAL_QSPI_TIMEOUT_DEFAULT_VALUE);
for(int i=0; i<size;i++)
{
HAL_QSPI_Transmit(&hqspi, &data[i], HAL_QSPI_TIMEOUT_DEFAULT_VALUE);
printf("sentdata:%0x",data[i]);
}
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, GPIO_PIN_SET);
printf("\n");
}
void QSPI_Read(uint32_t address, uint8_t *data, uint32_t size) {
QSPI_CommandTypeDef sCommand;
sCommand.InstructionMode = QSPI_INSTRUCTION_1_LINE;
sCommand.Instruction = READ_CMD;
sCommand.AddressMode = QSPI_ADDRESS_1_LINE;
sCommand.Address = address;
sCommand.DataMode = QSPI_DATA_4_LINES;
sCommand.NbData = 1;
sCommand.DummyCycles = 0;
sCommand.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, GPIO_PIN_RESET);
HAL_QSPI_Command(&hqspi, &sCommand, HAL_QSPI_TIMEOUT_DEFAULT_VALUE);
for(int i=0; i<size; i++)
{
HAL_QSPI_Receive(&hqspi, &data[i], HAL_QSPI_TIMEOUT_DEFAULT_VALUE);
printf("%0x",data[i]);
}
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, GPIO_PIN_SET);
printf("\n");
}
int main(void)
{
uint8_t dataToWrite[4] = {0x25,0x26,0x27,0x28};
// Write data to EEPROM
QSPI_Write(0x3, dataToWrite, sizeof(dataToWrite));
HAL_Delay(1000);
QSPI_Read(0x3, dataToRead, 4);
}
static void MX_QUADSPI_Init(void)
{
/* USER CODE BEGIN QUADSPI_Init 0 */
/* USER CODE END QUADSPI_Init 0 */
/* USER CODE BEGIN QUADSPI_Init 1 */
/* USER CODE END QUADSPI_Init 1 */
/* QUADSPI parameter configuration*/
hqspi.Instance = QUADSPI;
hqspi.Init.ClockPrescaler = 2;
hqspi.Init.FifoThreshold = 4;
hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_NONE;
hqspi.Init.FlashSize = 11;
hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_1_CYCLE;
hqspi.Init.ClockMode = QSPI_CLOCK_MODE_0;
hqspi.Init.FlashID = QSPI_FLASH_ID_1;
hqspi.Init.DualFlash = QSPI_DUALFLASH_DISABLE;
if (HAL_QSPI_Init(&hqspi) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN QUADSPI_Init 2 */
/* USER CODE END QUADSPI_Init 2 */
}
Solved! Go to Solution.
2025-01-06 9:10 AM
Then you might need to unpack things manually from the traces.
I would suggest starting with the QSPI in 1-bit interactions, reading the JEDEC ID and SFDP data from it. If you can get that to work you'll need to look at modes and methods to switch to 4-bit operation.
QSPI_CommandTypeDef sCommand = {0}; // strongly advised for large auto/local structures
If correctly wired and functional I'd anticipate PA2:AF10 QUADSPI_BK1_NCS, and multi-byte transmit/receiver to be viable
https://www.st.com/resource/en/datasheet/m95p32-i.pdf
2025-01-06 5:02 AM
Welcome to the forum.
Please see How to insert source code.
Also: How to write your question to maximize your chances to find a solution.
You haven't said what STM32 you're using, what board(s), or tool versions.
Are you using the X-CUBE-EEPRMA1 Standard I2C and SPI EEPROM software expansion for STM32Cube:
https://www.st.com/en/embedded-software/x-cube-eeprma1.html
via: https://www.st.com/en/ecosystems/x-nucleo-pgeez1.html#tools-software
and: https://www.st.com/en/memories/m95p32-i.html#tools-software
2025-01-06 5:17 AM
Hello @Gowthami412 and welcome to the community,
First as said by @Andrew Neil you need to use </> to paste your code. I've edited your post.
Second, which STM32 part number are you using?
2025-01-06 5:25 AM
Where do you call the initialization code?
Why manual PA2 chip select?
Why individual byte transfers?
Clear the sCommand structure as an auto/local variable.
Use a logic analyzer to confirm signaling on bus.
It is not designed to report all errors, just those it can detect at the HAL or peripheral level.
2025-01-06 8:38 AM
Ok Thank you. I am using STM Nucleo- L496ZGP board.
2025-01-06 8:41 AM
I am calling initialisation in int main I have initialized all required peripherals in main here I didn't paste.
1. I tried using without manual CS it didn't work, so I tried adding manual CS then also didn't work.
2. I tried sending all bytes at a time it didn't work, so I tried sending byte by byte.
3. We don't have a logic analyser with support QSPI to decode I tried
2025-01-06 9:10 AM
Then you might need to unpack things manually from the traces.
I would suggest starting with the QSPI in 1-bit interactions, reading the JEDEC ID and SFDP data from it. If you can get that to work you'll need to look at modes and methods to switch to 4-bit operation.
QSPI_CommandTypeDef sCommand = {0}; // strongly advised for large auto/local structures
If correctly wired and functional I'd anticipate PA2:AF10 QUADSPI_BK1_NCS, and multi-byte transmit/receiver to be viable
https://www.st.com/resource/en/datasheet/m95p32-i.pdf
2025-01-07 2:39 AM
Thank you for your suggestion. I am getting JEDEC ID and RDID with QSPI in 1 line mode. But while writing with 4 line mode it is not working.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.