STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F401 Interpreting DMA data over serial

Hi all,I am pretty new to ST so bear with me.The controller is reading in voltage values into the ADC and sending to PC over serial withCDC_Transmit_FS((uint8_t*), buffer, buffer_length)I'm getting the data stream, but the values as read in python fo...

STM32F401CCU6 Crashes in empty while loop.

HelloI am testing new MCU's. I have a ST-Link V2 and using a STM32F401CCU6.At the start I had a simple LED flasher application however after I could not run it I started stripping everything out.This is when I saw that I can actually not even run an ...

STM32Issue1.png STM32Issue2.png
table by Associate II
  • 1786 Views
  • 4 replies
  • 1 kudos

Resolved! CAN1 RX issue

Hi I am using STM32F407 evb in which I have configured both CAN1 and CAN2 ,I am sendind CAN1(3 ids 501,502,503) and vice versa from CAN2 same I am sending but I am ble to recive all three id on CAN2 Rx but only one ID iam receving on CAN1(501) .I am ...

Ash1 by Associate III
  • 6506 Views
  • 21 replies
  • 0 kudos

STMF32F401RE with IHM04A1

I am working with STM32F401RE and IHM04A1 driver board. There is timer1 channel 3 in EN-A (PA10) for IN1A and IN2A. However, there is no timer channel in EN-B which should be used for IN1B and IN2B. What should I do for the timer in EN-B, that is, PC...

aknaydn by Associate
  • 1928 Views
  • 4 replies
  • 0 kudos

Resolved! Configure crystal but using oscillator

Hello together, I have a question regarding the configuration of the HSE. We have a product which is running on a crystal, so we configured our HSE as "Crystal/Ceramic Resonator". In a new hardware revision our hardware team decided to use a active o...

ESawa.1 by Senior
  • 1158 Views
  • 1 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.