STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F2/F4 USB-MSC >4gb limitation

Posted on July 18, 2016 at 11:48 Hi. I have added USB Host support for MSC. It is working ok with USBs under 4gb... but it is not detected properly with USB-sticks over 4gb. I'm using library version 2.2.0, microcontroller are F2/F...

0690X000006039yQAA.jpg
pedro23 by Senior
  • 3210 Views
  • 6 replies
  • 0 kudos

Usart 2 interrupt problem STM32F303CC

Posted on December 08, 2014 at 16:06 Hello I'm using a STM32F303CC lqfp 48 on a new product. I'm trying to use 3 Usart channels. I succesfully use channel 1 and 3 but channel 2 is acting weird. In configure the three channels all in the s...

m_ by Associate II
  • 5446 Views
  • 10 replies
  • 0 kudos

DFSDM 8 serial channels but 4 filters. Why????

Posted on June 11, 2016 at 20:44I use the DFSDM in multichannel sound card USB. It is 1st time for me.I have read that the average DFSDM has 8 channels.When I started the project I have found that STM engineers added only 4 filters for 8 channels. I...

delphi by Associate II
  • 13228 Views
  • 41 replies
  • 0 kudos

CubeMX 4.16.0 download checksum is bad.

Posted on July 15, 2016 at 07:04Downloading the 4.16.0 update yields the error message in the attachment.The file checksum is wrong. I tried downloading about 6 times. Same result each time.You can also correct the wording in the error message. Let ...

Read analog Value from non ADC input (GPIO-Analog mode)

Posted on July 19, 2016 at 09:11Hello, I�m a bit confused about the documentation from the GPIOs. It says that all GPIO can be put in analog mode, so my assumption was that I could use all of them as analog input. However, nowhere in the GPIO chapt...

jbober by Associate
  • 697 Views
  • 0 replies
  • 0 kudos

stm32f103: synchronize a few timers

Posted on July 18, 2016 at 23:28Hi, I would like to control a brushless motor in gimbal project for this purpose I use three timers, but diffrent to one motor and I prepare timers as a PWM output and set a pulse which is out of phase, but because of...

STM32f207 PWM output

Posted on July 15, 2016 at 16:44Hi, I am trying to generate a PWM output on port PE9. I have set up the Timer configuration, the GPIO configuration and the interrupts. Somehow when I add the code to set up the PWM mode, then I completely lose my sig...

eugenia by Associate II
  • 1710 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.