2016-07-18 2:28 PM
Hi, I would like to control a brushless motor in gimbal project for this purpose I use three timers, but diffrent to one motor and I prepare timers as a PWM output and set a pulse which is out of phase, but because of I use different timers I dont have a good synchronization, how can I synchronize three timers TIM3->CCR1, TIM2->CCR4, TIM2->CCR3?
2016-07-18 3:55 PM
That would appear to describe TWO timers, each timer only has a single counting element, CNT, describing the current phase-angle of the timer across the period. The phase difference between CCR3 and CCR4 is in units of the baseline tick, defined by the APB/TIM CLK and the Prescaler.
You can put timers in a slave mode, and have them reset on an input trigger. You'd have to pick slave timers and configurations which share a common master so they all reset together.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.