STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to create eclipse project from scratch?

Posted on July 18, 2016 at 20:09Hi, I'm using SW4STM32 to play around with STM32F0-Discovery board. I know that ST has provided project templates for different tools. Whenever you create a project the project wizard gives you option to import the fi...

rsakaria by Associate
  • 1087 Views
  • 1 replies
  • 0 kudos

Firmware load instructions

Posted on July 15, 2016 at 15:44I have been dissecting my STM32L151's code. It starts at address 0800 0000 and consists of around 50 load instructions. After each load instruction, the value is shifted right by 0x20 and stored into R0. After each lo...

PWM Output on STM32F2XX (Solved)

Posted on February 02, 2012 at 14:30Greetings,I am currently toying around with the KEIL MCBSTM32F200 Evaluation Board(the STM32F207VG uC) and have run into some problems with the PWM output.I want a simple PWM-signal on TIM1, Channel1 (PA8 for STM3...

th2 by Associate
  • 5707 Views
  • 10 replies
  • 0 kudos

uCLinux in stm3210e-eval board

Posted on July 18, 2016 at 15:34Hello, I have STM3210e-eval board (ARM Cortex M3 core-based STM32F103ZGT6). In AN3012 Application Note (pag. 6 ''Package Description'') the section presents all the files in the package that are needed to get started ...

STM32Cube errata?

Posted on July 18, 2016 at 00:20Hi everyone,So I would like to test out a bit of the STM32Cube. But first I was looking for a bug list on current versions so I don't run into a stupid problem and get stuck for hours.Is there a errata for the STM32Cu...

Minimal response time for PID controller based on stm32f103

Posted on July 18, 2016 at 12:05In article http://jeelabs.org/article/1619b/ buffer acquisition time is 32ms with 800 samples. Is real to access frequently into buffer with taking few samples for smallest PID response time? Someone ''fast PID'' libr...

dimk95 by Associate
  • 1013 Views
  • 0 replies
  • 0 kudos

UART Transmit problem

Posted on July 16, 2016 at 09:55Hello!I'm working on UART comunication between stm32f407 and PC. I want to transmit 4 character via ''senddata()'' function shown below.USART_SendData(USART1,'D');while(USART_GetFlagStatus(USART1, USART_FLAG_TC)==RESE...

STM32f207 remapping pins problem

Posted on July 10, 2013 at 17:17 I'm not sure how to remap pins that do not line up correctly with the alternate functions specified in the datasheet. For example, the picture below shows the pin out of my microcontroller where OCx-LOW are pwm o...

0690X00000604woQAA.png 0690X00000604lDQAQ.png
dbingle by Associate II
  • 7147 Views
  • 20 replies
  • 0 kudos

STM32L476 input capture

Posted on July 13, 2016 at 14:08 Hello, I am working with the boardNucleo-L476RG and I wantto capture frequency on the pin PA0 with TIM2 Channel1. My timer is working but I can't get the interrupt in the function TIM2_IRQHandler(). I a...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.