STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC DC ''crosstalk'' between channels

Posted on July 19, 2016 at 16:53Hello, I use STM32L152 on STs Nucleo board. I created a small progtam to test ADC. It is mainly a state machine that steps forward every 100msec, repeating after 10 steps. In step 1 I start a conversion sequence cons...

mmensch by Associate II
  • 2859 Views
  • 2 replies
  • 0 kudos

LCD Scroll Slow with SDRAM as System Ram

Posted on July 20, 2016 at 10:32I'using STM32746G-Discovery boardkeil 5.20STM32F7xx_DFP/2.7.0I do some test with LwIP_HTTP_Server_Netconn_RTOS examples. This example use: -    LwIp Library -    LCD interface with the framebuffer mappend on the S...

ruggero by Associate
  • 604 Views
  • 0 replies
  • 0 kudos

STM32L073 SPI CRC calculation

Posted on July 19, 2016 at 09:06 I am using SPI to communicate with an external NVM memory and hope to have some data validate at the end by using CRC. But I do not understand how does the SPI CRC calculation contribute to verify the data that I...

waiyang93 by Associate II
  • 3330 Views
  • 3 replies
  • 0 kudos

Could someone explain this ''Reset Handler''?

Posted on July 20, 2016 at 00:08I am using Keil uVision, and occasionally, at start of debug, the program counter would stuck at the Rest handler routine below.  The execution would point to the instruction:       ''BLX      R0''  (line #2) and woul...

Vu.Andy by Associate III
  • 5121 Views
  • 3 replies
  • 0 kudos

STM32F4 timer driven DMA

Posted on July 19, 2016 at 13:32  The original post was too long to process during our migration. Please click on the attachment to read the original post.

STM32F407VGT6 external oscillator

Posted on July 19, 2016 at 13:19Hi everyone, I have designed a board using stm32f407vgt6 and placed a 8MHz crystal oscillator with 22pF capacitors. The code I wrote works perfectly with stm32f4discovery. But when I try to use my board, it can't init...

DMA problem ?

Posted on July 19, 2016 at 13:58Dear All,I am facing a strange problem. I am using a slave SPI to transfer memory data by a DMA stream. The transfer uses 16-bit wide data. On the stm32f429 (m4) the code works very well and I can use the data. The sa...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.