STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SVS in ARM Micro-controllers

Posted on October 05, 2016 at 15:26Unfortunately, I am sort of thinking of using SVS (Supply Voltage Supervisor) in my STM32f107kc. Why am I saying like this. Because, I am not entirely too sure my flash store my data without having power. Assuming ...

18msps sampling in stm32f303 48/64 pin packages

Posted on October 03, 2016 at 08:15Helloaccording to stm32f303cb datasheet, 48 pin package doesn't have ADC12/34 shared channels.If one needs to sample an input with 18msps in dual interleaved mode, how it will be possible in 48 pin package? is it p...

Overclocking STM32F4

Posted on October 04, 2016 at 01:09Does anyone have any experience in overclocking an STM32F4 to 240MHz?  Is that an ST recommended configuration?  I've run across a new product being sold that advertises that they are overclocking to 240MHz by reco...

webbbn by Associate
  • 2626 Views
  • 3 replies
  • 0 kudos

Minimal circuit for STM32F407

Posted on October 01, 2016 at 01:40DearI'm new with STM32 MCU and would like some expert help me with the minimum circuit (oscillator, power supply with Vinput 9-32V DC, reset, etc.). I just need to connect an SPI device and CANBUS driver. I should ...

[STM32L4] timer interrupt starts immediately

Posted on October 04, 2016 at 13:07Hi, using TIM1 to get a simple 1ms delay (MCU@24MHz, PSC=24, ARR=1000) the interrupt triggers almost as soon as I set CR1:CEN=1. I've found that I'm not the only one having this problem, have followed the advice gi...

Noyb by Associate II
  • 4057 Views
  • 9 replies
  • 0 kudos

STM32f429-Discovery Ili9341 Lib

Posted on October 05, 2016 at 09:45HelloI downloaded STM32Cube_FW_F4_V1.13.0 but I wonder how I can migratethe ILI9341 Lib with a Cube Project ?

ats3788 by Associate II
  • 1422 Views
  • 2 replies
  • 0 kudos

RTC clock source

Posted on October 03, 2016 at 01:46Hello, I'm a little confused about choosing the better clock source for the RTC, is it better to drive it through HSE with 4MHz 10ppm frequency tolerance or using additional 32.768KHz LSE with also 10ppm tolerance?...

Disabling IRQ causes irq routine to be called

Posted on October 04, 2016 at 12:20 Hi, I found something curious (for me...) while playing around usart interrupts on STM32L1 // USART1 is initialized and IRQ is enabled // TC is 1 // TCIE is 0 __HAL_UART_ENABLE_IT(&huart1,...

JulienD by Senior
  • 787 Views
  • 1 replies
  • 0 kudos

Sampling ADC data

Posted on October 04, 2016 at 19:55I'm trying to get data from an ADC7689,  using SPI. I have a NUCLEO STM31F411RE and the code is running on SW4STM32. My problem is that when I send addresses, all I get is 0xFF, instead of the values the ADC conve...

marco3 by Associate II
  • 957 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.