2016-10-02 11:15 PM
Hello
according to stm32f303cb datasheet, 48 pin package doesn't have ADC12/34 shared channels.
If one needs to sample an input with 18msps in dual interleaved mode, how it will be possible in 48 pin package? is it possible to connect two pins (e.g. ADC1_IN1 & ADC2_IN1) externally?
2016-10-05 8:02 AM
Hi tag.aseok,
Yes, You can connect the signal to the 2 input pins, to reach the 18MSPS with a 6-bit resolution. But for the 12-bit resolution case, 10MSPS is the maximum sampling.-Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.