2016-10-04 3:20 AM
Hi,
I found something curious (for me...) while playing around usart interrupts on STM32L1// USART1 is initialized and IRQ is enabled
// TC is 1
// TCIE is 0
__HAL_UART_ENABLE_IT(&huart1, UART_IT_TC); -- > none interrupt routine is called
HAL_NVIC_DisableIRQ(USART1_IRQn); ---> USART1_IRQHandler is called
After standard initialization of usart1 with cubeMx (containing a call to
HAL_NVIC_EnableIRQ(USART1_IRQn); ).
TC flag is 1 and TCIE flag is 0. So none interrupt is called. Now here's the point:
When I call
__HAL_UART_ENABLE_IT(&huart1, UART_IT_TC);
none interrupt routine is called while I think it should because TC is 1.
Then, when I call
HAL_NVIC_DisableIRQ(USART1_IRQn); ---> USART1_IRQHandler is called
USART1_IRQHandler is called while I think it should not.
Is it a regular behaviour? If yes, is there a reason?
Thanks
Julien
#stm32l1-interrupt-usart
2016-10-04 3:34 PM
Hum, forget this question for the moment.
I implemented this on an eval board and I don't reproduce... I'll reduce the non working code and may be get back with more info. JulienWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.