2016-10-04 4:07 AM
Hi, using TIM1 to get a simple 1ms delay (MCU@24MHz, PSC=24, ARR=1000) the interrupt triggers almost as soon as I set CR1:CEN=1.
I've found that I'm not the only one having this problem, have followed the advice given here and there, but still no luck. 1- Start peripheral (RCC) 2- Reset peripheral 3- Set registers (SR, CR1, SMCR, BDTR, CNT, ARR, PSC) 4- Do some read back to ensure propagation 5- Tried the EGR:UG=1 trick 6- Tried the CR1:URS=1 trick 7- Interrupt is cleared at the beginning of the ISR 8- Start the timer, interrupt triggers within 50us (about 1200 cycles) This is rather hard to get this thing working without deploying a whole army. #stm32l4-timer-interrupt-spurious #stm32l4-timer-interrupt-spurious #stm32l4-timer-interrupt-spurious #stm32l4-timer-interrupt-spurious #stm32l4-timer-interrupt-spurious2016-10-04 4:24 AM
Which interrupt?
Post code. JW2016-10-04 5:11 AM
Can' post code, too complicated, not MX stuff, scattered all over several files.
1- RCC->APB2ENR |= RCC_APB2ENR_TIM1EN 2- RCC->APB2RSTR |= RCC_APB2RSTR_TIM1RST 3- RCC->APB2RSTR &= ~RCC_APB2RSTR_TIM1RST 4- TIM->CR1 |= (TIM_CR1_URS) (trick ?) 5- TIM->SR = 0, tim_sr = TIM->SR (read back) 6- TIM->CR1 = 0 7- TIM->SMCR = 0 8- TIM->BDTR = TIM_BDTR_MOE 9- TIM->CNT = 0 10- TIM->ARR = 1000 - 1 (1000us) 11- TIM->PSC = 24 - 1, tim_psc = TIM->PSC (read back) 12- TIM->RCR = 0 13- TIM->EGR &= TIM_EGR_UG (trick ?) 14- TIM->DIER = TIM_DIER_UIE 15- NVIC_ClearPendingIRQ(TIM1_UP_TIM16_IRQn) & (TIM1_CC_IRQn) 16- NVIC_SetPriority(TIM1_UP_TIM16_IRQn) & (TIM1_CC_IRQn) 17- NVIC_EnableIRQ(TIM1_UP_TIM16_IRQn) & (TIM1_CC_IRQn) -> could triggers here 18- TIM->CR1 &= ~(TIM_CR1_URS) (trick ?) 19- TIM->CR1 |= (TIM_CR1_OPM) 20- TIM->SR = 0, tim_sr = TIM->SR (yeah, to be sure) 21- TIM->CR1 |= (TIM_CR1_CEN) 22- Boom! after 50us instead of 1000us :\2016-10-04 5:26 AM
> TIM->EGR &= TIM_EGR_UG (trick ?)
No, this won't do the trick. You need to *set* TIM_EGR.UG. JW2016-10-04 6:43 AM
> TIM->EGR &= TIM_EGR_UG (trick ?)
No, this won't do the trick. You need to *set* TIM_EGR.UG. JW2016-10-04 6:49 AM
Could you post your correction to my code flow?
2016-10-04 7:05 AM
> Could you post your correction to my code flow?
>>> TIM->EGR &= TIM_EGR_UG (trick ?)
>> No, this won't do the trick. You need to *set* TIM_EGR.UG.TIM->EGR = TIM_EGR_UG;
JW2016-10-04 7:45 AM
Nope, doesn't work, already tried that.
It appears that the counter doesn't even start counting when CR1:CEN=1 because when reading CNT it remains at 0. However the interrupt is triggered just after that. When using TIM3 CH4 for PWM, no problem, CNT runs fine after CR1:CEN=1 :\2016-10-04 8:07 AM
> Nope, doesn't work, already tried that.
WHAT doesn't work? What did you try already? > It appears that the counter doesn't even start counting when CR1:CEN=1 because when reading CNT it remains at 0. Reading how? Can't this be because of the one-pulse mode you set? Create a simple but complete, compilable example reproducing the problem, and post that.2016-10-05 3:04 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.