2016-10-05 6:26 AM
Unfortunately, I am sort of thinking of using SVS (Supply Voltage Supervisor) in my STM32f107kc. Why am I saying like this. Because, I am not entirely too sure my flash store my data without having power. Assuming it does not so, I am familiar with SVS in MSP micro-controllers. However, in STM32f107kc as I found out I have the following registers to control the power.
/******************************************************************************//* *//* Power Control *//* *//******************************************************************************//******************** Bit definition for PWR_CR register ********************/&sharpdefine PWR_CR_LPDS ((uint16_t)0x0001) /*!< Low-Power Deepsleep */&sharpdefine PWR_CR_PDDS ((uint16_t)0x0002) /*!< Power Down Deepsleep */&sharpdefine PWR_CR_CWUF ((uint16_t)0x0004) /*!< Clear Wakeup Flag */&sharpdefine PWR_CR_CSBF ((uint16_t)0x0008) /*!< Clear Standby Flag */&sharpdefine PWR_CR_PVDE ((uint16_t)0x0010) /*!< Power Voltage Detector Enable */&sharpdefine PWR_CR_PLS ((uint16_t)0x00E0) /*!< PLS[2:0] bits (PVD Level Selection) */&sharpdefine PWR_CR_PLS_0 ((uint16_t)0x0020) /*!< Bit 0 */&sharpdefine PWR_CR_PLS_1 ((uint16_t)0x0040) /*!< Bit 1 */&sharpdefine PWR_CR_PLS_2 ((uint16_t)0x0080) /*!< Bit 2 *//*!< PVD level configuration */&sharpdefine PWR_CR_PLS_2V2 ((uint16_t)0x0000) /*!< PVD level 2.2V */&sharpdefine PWR_CR_PLS_2V3 ((uint16_t)0x0020) /*!< PVD level 2.3V */&sharpdefine PWR_CR_PLS_2V4 ((uint16_t)0x0040) /*!< PVD level 2.4V */&sharpdefine PWR_CR_PLS_2V5 ((uint16_t)0x0060) /*!< PVD level 2.5V */&sharpdefine PWR_CR_PLS_2V6 ((uint16_t)0x0080) /*!< PVD level 2.6V */&sharpdefine PWR_CR_PLS_2V7 ((uint16_t)0x00A0) /*!< PVD level 2.7V */&sharpdefine PWR_CR_PLS_2V8 ((uint16_t)0x00C0) /*!< PVD level 2.8V */&sharpdefine PWR_CR_PLS_2V9 ((uint16_t)0x00E0) /*!< PVD level 2.9V */&sharpdefine PWR_CR_DBP ((uint16_t)0x0100) /*!< Disable Backup Domain write protection *//******************* Bit definition for PWR_CSR register ********************/&sharpdefine PWR_CSR_WUF ((uint16_t)0x0001) /*!< Wakeup Flag */&sharpdefine PWR_CSR_SBF ((uint16_t)0x0002) /*!< Standby Flag */&sharpdefine PWR_CSR_PVDO ((uint16_t)0x0004) /*!< PVD Output */&sharpdefine PWR_CSR_EWUP ((uint16_t)0x0100) /*!< Enable WKUP pin */That I am not familiar with them entirely. On the other hand, in MSP I had to have the following code to enable SVS.if (SVSCTL&SVSFG){ // If the power goes off
FlshCarma( total_consumed_active_energy ); // Store the lost number here
SVSCTL |= PORON; // enable POR
}
So, I am just wondering what are the major registers I am required to use to enable my SVS in ARM. Any working examples you may suggest?Thanks! #stm32f #svs2016-10-05 9:55 AM
Hi CaEngineer,
The device features an embedded programmable voltage detector (PVD) that monitors theVDD/VDDA power supply and compares it to the VPVD threshold. An interrupt can be generated when VDD/VDDA drops below the VPVD threshold and/or when VDD/VDDA is higher than the VPVD threshold. The interrupt service routine can then generate a warning message and/or put the MCU into a safe state. The PVD is enabled by software.I think you are using the , you would check the PVD firmware example at this path: STM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPeriph_Examples\PWR\PVD-Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.