STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! AN2606 Rev 70 pin description bugs

Hi,When reviewing the descrption of MCU pins used by the integrated system bootloader, I came across several documentation bugs in the latest AN2606 (rev70). Inparticular, Table 164 lists:USART1_TX pin - PA9 pin: USART1 in transmission mode. Used in ...

Resolved! STM32H7R7Z8 XSPI has timing issue in Quad mode

Hi, EveryoneI am trying to setup STM32H7R7Z8 XSPI2 in Quad mode for APS6404L-3SQR QSPI PSRAM.The original code is generated from MX v6.116.1 and developed with IDE v2.0.0.HW info:The PSRAM is connected to XSPI2 with NCS, CLK, IO0~3. There is no DQS p...

xspi-register.png
Leo2Ruan by Associate III
  • 627 Views
  • 6 replies
  • 0 kudos

Unable to configure hardware SPI 1

Hi I am trying to set up hardware SPI using the following. My software SPI works fine, but the hardware SPI doesn't even have a clock signal.   /** ****************************************************************************** * @file : main.c * @...

Amirreza by Associate
  • 324 Views
  • 1 replies
  • 0 kudos

Resolved! STM32N6 Can't program due to BOOT1 pin tied to ground

Hi, I have a custom STM32N6 board where the BOOT0 and BOOT1 pins are tied directly to ground under the BGA with no test points or jumpers. Is there anyway to connect a debugger in this scenario or is my board bricked? Below is what I get when attempt...

ben5050 by Associate II
  • 644 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.