STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Internal Temp Sensor STM32H563VI

Dear ST Community,I am currently migrating my Firmware from STM32H723VG to STM32H563VI. I have problem with Internal Temp Sensor. Based on Reference Manual on both MCU reading temperature is the same, but it doesn't work as it should.When on STM32H7 ...

adakPal by Associate III
  • 554 Views
  • 6 replies
  • 2 kudos

Resolved! Timer cascading not working as expected

I'm working on a design with an STM32L072CZT6TR, where I want to calibrate my main timebase. That main timebase is TIM6, which counts 16,000. The HSE is 16MHz, so there's an interrupt evey 1ms. Calibration is done by counting the number of HSE cycles...

RobK1 by Senior II
  • 304 Views
  • 2 replies
  • 1 kudos

Resolved! CAN BUS on Nucleo H743ZI2 - clock configuration issue

Hello,I’ve recently started using ST products and the IDE with CubeMX, which is why I’m asking for your help. I’ve just begun developing a communication system using a Nucleo H743ZI2; my goal is to set up a UART and a CAN bus.The UART is done; I used...

Forum_ST_1.png Forum_ST_2.png
AmGo by Associate III
  • 939 Views
  • 12 replies
  • 8 kudos

Resolved! Does STM32G0B1KBU6 Support PD 3.1

According to the PD 3.1 requirements (also PD 3.0), I need to connect UCPD1_CC1 and UCPD1_CC2 to USB-C CC1 and CC2 to communicate and request the desired voltage. But STM32G0B1KBU6  has only UCPD1_CC1 available. Is there any way to connect STM32G0B1K...

HDKLog by Associate
  • 256 Views
  • 1 replies
  • 0 kudos

STM32L071 Operation Failure and Power Line Resistance

Hello.I recently experienced an unusual MCU Problem and need to analyze it. Please help me. The FW program download to the MCU is successful, but it does not operate after a reset. I performed a short circuit test after disconnecting the power(Batter...

JinMoon by Associate
  • 298 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.