STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Some Bootloader questions

I had a question regarding the bootloader, more specifically, the for the F429 variant. On app note AN2606, they list the embedded bootloaders. For the F42XXX and F43XXX variants, they list two different bootloader ID's. How do you know which one you...

AndrewC_0-1737989398267.png AndrewC_1-1737989993555.png
Andrew C by Associate III
  • 1404 Views
  • 1 replies
  • 0 kudos

Resolved! SPI as master and FPGA as slave for some bits

Hello everybody. I asking now for some help on my new project. On my stm32 u575zit-q i want send some bits, as master, on the FPGA EP2C5T144C8N as slave. This FPGA board is very simple (have no other peripherals on it). So i want send by means SPI, f...

SMusc.1 by Senior
  • 4403 Views
  • 14 replies
  • 3 kudos

PSSI and DMA issue

Hi,I am using PSSI on STM32H7R3 to transmit data with DE output signal and RDY input signal (flow control). Incoming clock frequency is 60MHz. Data buffer is located in AHBSRAM1 and have size 4096 bytes. GPDMA feeds PSSI buffer by 32bit access (four ...

error2.png error1.png error3.png ok3.png

Resolved! Multi Channel ADC with DMA on a NUCLEO H753ZIT6

I'm just getting started with STM32 microcontrollers and I have been using the NUCLEO H753ZIT6. I was trying to learn how to use multiple channels of ADC's with DMA. I was able to get some data when I used a single channel ADC normally. But now I'm n...

USB host issue in CDC mode

Hello everyone,I am developing firmware for the STM32F7508-DK discovery board, and I'm utilizing TouchGFX for the GUI aspect of the project. However, I am encountering a problem when enabling USB-FS HOST functionality. The GUI and other peripherals s...

iSaeed62 by Associate II
  • 1728 Views
  • 1 replies
  • 0 kudos

STM32WB5MM CPU2 bootup issue if image of CPU1 is relocated

Hi,I am using stm32WB5MM, I have bootloader which is located on regular start address 0x8000000.Bootloader executes image which is located on some other location (location is divisible by 0x400 as required).For that image I changed linker file and xx...

zax by Associate II
  • 944 Views
  • 1 replies
  • 0 kudos

Reduce Current consumption upto 3.8mA

Configured the controller stm32l151c8t6a to work in low power run mode ( UART peripheral running) but the current consumption is going upto 6.2mA. After disabling the uart peripheral the consumption decreases upto 4.2mA. In real situation we are goin...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.