2025-01-24 5:23 AM - edited 2025-01-24 5:28 AM
I'm just getting started with STM32 microcontrollers and I have been using the NUCLEO H753ZIT6. I was trying to learn how to use multiple channels of ADC's with DMA. I was able to get some data when I used a single channel ADC normally. But now I'm not even able to get any data when I put the ADC data storing array in the "Live Expressions" tab. I have also tried to use timers to make the ADC conversions happen at a frequency of 10Hz. I have attached images of how I've setup the ADC and Timer. My timer configuration has a prescaler of 64000-1 because the Timer clock is running at 64 MHz. My ADC is running at a clock of 40 MHz because I thought if its less then it may work. I have also tried the "Continuous Conversion Mode" in the ADC setting and the "Circular mode" in the DMA setting but none of them work. This is my main.c file:
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2025 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define ADC_BUFSIZE 20
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc3;
DMA_HandleTypeDef hdma_adc3;
TIM_HandleTypeDef htim2;
/* USER CODE BEGIN PV */
uint32_t ADC_BUFFER[ADC_BUFSIZE];
uint8_t adc_ready = 0;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_BDMA_Init(void);
static void MX_ADC3_Init(void);
static void MX_TIM2_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* Enable the CPU Cache */
/* Enable I-Cache---------------------------------------------------------*/
SCB_EnableICache();
/* Enable D-Cache---------------------------------------------------------*/
SCB_EnableDCache();
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_BDMA_Init();
MX_ADC3_Init();
MX_TIM2_Init();
/* USER CODE BEGIN 2 */
HAL_ADCEx_Calibration_Start(&hadc3, ADC_CALIB_OFFSET, ADC_SINGLE_ENDED);
HAL_ADC_Start_DMA(&hadc3, ADC_BUFFER, ADC_BUFSIZE);
HAL_TIM_Base_Start(&htim2);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
while(adc_ready != 1){
}
adc_ready = 0;
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Macro to configure the PLL clock source
*/
__HAL_RCC_PLL_PLLSOURCE_CONFIG(RCC_PLLSOURCE_HSI);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV1;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief ADC3 Initialization Function
* @PAram None
* @retval None
*/
static void MX_ADC3_Init(void)
{
/* USER CODE BEGIN ADC3_Init 0 */
/* USER CODE END ADC3_Init 0 */
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC3_Init 1 */
/* USER CODE END ADC3_Init 1 */
/** Common config
*/
hadc3.Instance = ADC3;
hadc3.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV2;
hadc3.Init.ScanConvMode = ADC_SCAN_ENABLE;
hadc3.Init.EOCSelection = ADC_EOC_SEQ_CONV;
hadc3.Init.LowPowerAutoWait = DISABLE;
hadc3.Init.ContinuousConvMode = ENABLE;
hadc3.Init.NbrOfConversion = 2;
hadc3.Init.DiscontinuousConvMode = DISABLE;
hadc3.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T2_TRGO;
hadc3.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
hadc3.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR;
hadc3.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hadc3.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
hadc3.Init.OversamplingMode = DISABLE;
hadc3.Init.Oversampling.Ratio = 1;
if (HAL_ADC_Init(&hadc3) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_5;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
sConfig.OffsetSignedSaturation = DISABLE;
if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_4;
sConfig.Rank = ADC_REGULAR_RANK_2;
if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC3_Init 2 */
/* USER CODE END ADC3_Init 2 */
}
/**
* @brief TIM2 Initialization Function
* @PAram None
* @retval None
*/
static void MX_TIM2_Init(void)
{
/* USER CODE BEGIN TIM2_Init 0 */
/* USER CODE END TIM2_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
/* USER CODE BEGIN TIM2_Init 1 */
/* USER CODE END TIM2_Init 1 */
htim2.Instance = TIM2;
htim2.Init.Prescaler = 16000-1;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = 1000-1;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_ENABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM2_Init 2 */
/* USER CODE END TIM2_Init 2 */
}
/**
* Enable DMA controller clock
*/
static void MX_BDMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_BDMA_CLK_ENABLE();
/* DMA interrupt init */
/* BDMA_Channel0_IRQn interrupt configuration */
HAL_NVIC_SetPriority(BDMA_Channel0_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(BDMA_Channel0_IRQn);
}
/**
* @brief GPIO Initialization Function
* @PAram None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOF_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOE_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOB, LD1_Pin|LD3_Pin, GPIO_PIN_RESET);
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);
/*Configure GPIO pin : B1_Pin */
GPIO_InitStruct.Pin = B1_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pins : LD1_Pin LD3_Pin */
GPIO_InitStruct.Pin = LD1_Pin|LD3_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/*Configure GPIO pins : STLINK_RX_Pin STLINK_TX_Pin */
GPIO_InitStruct.Pin = STLINK_RX_Pin|STLINK_TX_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF7_USART3;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
/*Configure GPIO pin : LD2_Pin */
GPIO_InitStruct.Pin = LD2_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(LD2_GPIO_Port, &GPIO_InitStruct);
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
{
/* Prevent unused argument(s) compilation warning */
UNUSED(hadc);
adc_ready = 1;
HAL_ADC_Stop_DMA(&hadc3);
/* NOTE : This function should not be modified. When the callback is needed,
function HAL_ADC_ConvCpltCallback must be implemented in the user file.
*/
}
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @PAram file: pointer to the source file name
* @PAram line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
Solved! Go to Solution.
2025-01-25 7:16 AM
I see BDMA, seems like error.
Anyway, start from this example
https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H743I-EVAL/Examples/ADC
743 pretty much the same as 753.
2025-01-24 6:19 AM - edited 2025-01-24 6:20 AM
Hello @LopsidedCoder and welcome to the community,
Better to attach your ioc file instead of posting the screenshots of your configs and may be better to post a sketch of what do you want to achieve.
2025-01-24 1:11 PM
Do the values show up in the array if you pause and examine with the Expressions tab?
Live Expressions is known to behave poorly.
2025-01-25 1:04 AM
Thanks for responding! I examined it with the Expressions tab and i got an Error: Target not available. I added a few breakpoints and it was normal till this line:
HAL_ADC_Start_DMA(&hadc3, ADC_BUFFER, ADC_BUFSIZE);But when I went to the next breakpoint which was:
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
{
/* Prevent unused argument(s) compilation warning */
UNUSED(hadc);
adc_ready = 1;
HAL_ADC_Stop_DMA(&hadc3);
/* NOTE : This function should not be modified. When the callback is needed,
function HAL_ADC_ConvCpltCallback must be implemented in the user file.
*/
}it gave the target not found error.
2025-01-25 7:16 AM
I see BDMA, seems like error.
Anyway, start from this example
https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H743I-EVAL/Examples/ADC
743 pretty much the same as 753.
2025-01-27 4:39 AM
Hi, Thanks for the reply. I followed the Sample Code and it worked. I just had a small question, do we have to also include the configuration parameters like this:
AdcHandle.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV2; /* Asynchronous clock mode, input ADC clock divided by 2*/
AdcHandle.Init.Resolution = ADC_RESOLUTION_16B; /* 16-bit resolution for converted data */
AdcHandle.Init.ScanConvMode = DISABLE; /* Sequencer disabled (ADC conversion on only 1 channel: channel set on rank 1) */
AdcHandle.Init.EOCSelection = ADC_EOC_SINGLE_CONV; /* EOC flag picked-up to indicate conversion end */
AdcHandle.Init.LowPowerAutoWait = DISABLE; /* Auto-delayed conversion feature disabled */
AdcHandle.Init.ContinuousConvMode = ENABLE; /* Continuous mode enabled (automatic conversion restart after each conversion) */
AdcHandle.Init.NbrOfConversion = 1; /* Parameter discarded because sequencer is disabled */
AdcHandle.Init.DiscontinuousConvMode = DISABLE; /* Parameter discarded because sequencer is disabled */
AdcHandle.Init.NbrOfDiscConversion = 1; /* Parameter discarded because sequencer is disabled */
AdcHandle.Init.ExternalTrigConv = ADC_SOFTWARE_START; /* Software start to trig the 1st conversion manually, without external event */
AdcHandle.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; /* Parameter discarded because software trigger chosen */
AdcHandle.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR; /* ADC DMA circular requested */
AdcHandle.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN; /* DR register is overwritten with the last conversion result in case of overrun */
AdcHandle.Init.OversamplingMode = DISABLE; /* No oversampling */and this?
/* ### - 3 - Channel configuration ######################################## */
sConfig.Channel = ADCx_CHANNEL; /* Sampled channel number */
sConfig.Rank = ADC_REGULAR_RANK_1; /* Rank of sampled channel number ADCx_CHANNEL */
sConfig.SamplingTime = ADC_SAMPLETIME_810CYCLES_5; /* Sampling time (number of clock cycles unit) */
sConfig.SingleDiff = ADC_SINGLE_ENDED; /* Single-ended input channel */
sConfig.OffsetNumber = ADC_OFFSET_NONE; /* No offset subtraction */
sConfig.Offset = 0; /* Parameter discarded because offset correction is disabled */I already do this setup in the IOC file's ADC parameters. Either way, I was able to get the readings in the Live Expressions tab for every 2 index of the array because I had only initialized two channels of ADC1(and one of the sensors weren't working, so i got a 0 reading from it), so im guessing the two sensors were filling up the array after each loop. I also did the sConfig configuration thing for both channels i just wanted to know if i need to do that or the setup i do in the IOC file is enough.
2025-01-27 4:48 AM
@MasterT wrote:
I see BDMA, seems like error.
Indeed.
@LopsidedCoder see this article
2025-01-27 5:01 AM
Understood, thanks a lot! I'm still a bit confused if I have to code the ADC configuration parameters or if its the same as doing it in the IOC file.
2025-01-27 5:07 AM
@LopsidedCoder wrote:AdcHandle.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV2; /* Asynchronous clock mode, input ADC clock divided by 2*/ AdcHandle.Init.Resolution = ADC_RESOLUTION_16B; /* 16-bit resolution for converted data */ AdcHandle.Init.ScanConvMode = DISABLE; /* Sequencer disabled (ADC conversion on only 1 channel: channel set on rank 1) */ AdcHandle.Init.EOCSelection = ADC_EOC_SINGLE_CONV; /* EOC flag picked-up to indicate conversion end */ AdcHandle.Init.LowPowerAutoWait = DISABLE; /* Auto-delayed conversion feature disabled */ AdcHandle.Init.ContinuousConvMode = ENABLE; /* Continuous mode enabled (automatic conversion restart after each conversion) */ AdcHandle.Init.NbrOfConversion = 1; /* Parameter discarded because sequencer is disabled */ AdcHandle.Init.DiscontinuousConvMode = DISABLE; /* Parameter discarded because sequencer is disabled */ AdcHandle.Init.NbrOfDiscConversion = 1; /* Parameter discarded because sequencer is disabled */ AdcHandle.Init.ExternalTrigConv = ADC_SOFTWARE_START; /* Software start to trig the 1st conversion manually, without external event */ AdcHandle.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; /* Parameter discarded because software trigger chosen */ AdcHandle.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR; /* ADC DMA circular requested */ AdcHandle.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN; /* DR register is overwritten with the last conversion result in case of overrun */ AdcHandle.Init.OversamplingMode = DISABLE; /* No oversampling */and this?
/* ### - 3 - Channel configuration ######################################## */ sConfig.Channel = ADCx_CHANNEL; /* Sampled channel number */ sConfig.Rank = ADC_REGULAR_RANK_1; /* Rank of sampled channel number ADCx_CHANNEL */ sConfig.SamplingTime = ADC_SAMPLETIME_810CYCLES_5; /* Sampling time (number of clock cycles unit) */ sConfig.SingleDiff = ADC_SINGLE_ENDED; /* Single-ended input channel */ sConfig.OffsetNumber = ADC_OFFSET_NONE; /* No offset subtraction */ sConfig.Offset = 0; /* Parameter discarded because offset correction is disabled */
You can configure and generate that code with CubeMx.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.