STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Issue placing constants in flash

Posted on November 21, 2016 at 16:00 I'm following the post on[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/How%20to%20allocate%20variable%20in%20Flash%20to%...

Extract Some Data From A Signal By Timer

Posted on November 20, 2016 at 01:33Hi Guysi have a board(a) and this board send some async data with clock to my stm32f4 device.in this data transferred by board(a) have some dummy clock and i want reject this dummy clock.i want to capture input cl...

0690X00000603DCQAY.jpg
eittinfo by Associate II
  • 964 Views
  • 2 replies
  • 0 kudos

Mutex never received

Posted on November 19, 2016 at 23:50 Hey guys, I'm having some problems with mutexes. I'd like to take a mutex but could never obtain it. Not even directly at startup. my function looks like this USB_ERROR_LIST creat...

STM32F030 Read protect

Posted on November 21, 2016 at 09:49Hi Support,I would like to confirm that by setting register OB->RDP = 0x11; in my source code will stop read action ONLY from being performed when using the RS232 bootloader. If i needed to do firmware updates usi...

older versions of cubemx and cube firmware libraries

Posted on November 21, 2016 at 15:39Hi,Is there somewhere I can obtain older versions of cubeMX and the cube firmware libraries?since ST doesn't seem to maintain backward compatibility, I need cubeMX v4.14.0 and the stm32f4 cube library v1.11.0Thank...

leet1 by Associate II
  • 1478 Views
  • 3 replies
  • 0 kudos

STM32F4XX PA0 WKUP from STANDBY issue

Posted on November 21, 2016 at 15:42I am having unreliable behavior with PA0 wakeup the chip from standby. If I just did a cold power cycle, the WKUP works, after I do several cycles ofWKUP--RUN APPLICATION--GOTO STANDBYthe chip does not wakeup or r...

Bug CubeMX 4.17 STM32F303 after emigration

Posted on October 14, 2016 at 11:12 Hello. i am using Cube MX 1.17 and the firmware package 1.6 on the STM32F303xC. After emigration from the related CubeMX version to the new i am getting a syntax error by new compiling the code. Th...

tino1 by Associate II
  • 4116 Views
  • 9 replies
  • 0 kudos

Solved! - Stm32CubeMX - UART - DMA - ERROR DETECTION

Posted on October 08, 2015 at 00:01 Hi, I have a problem in catching errors when using UART in DMA mode.  I use CubeMx to generate the code.   The functions which I use to catch interrupts are the following (obviously my code is more complex, this ...

silvio1 by Associate
  • 2412 Views
  • 3 replies
  • 0 kudos

Problem entering Standby mode STM32L051

Posted on November 18, 2016 at 14:45Hi all,I have an odd behavior on my STM32L051 trying to enter in STANDBY mode.  I would be pleased if you could help me. My program repeat endless cycles activity and Standby.Once the firmware boot and after some ...

During Build I get this: [Src/main.o] Error 2

Posted on November 21, 2016 at 00:35I am trying to develop an application on a STM32L476 Nucleo 64 development board.  I get this error after the Build using the STM32 System Workbench IDE with standard default settings.  I set up the project using ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.