2016-11-21 6:42 AM
I am having unreliable behavior with PA0 wakeup the chip from standby. If I just did a cold power cycle, the WKUP works, after I do several cycles of
WKUP--RUN APPLICATION--GOTO STANDBYthe chip does not wakeup or respond to the PA0 pulse anymore. I suspect the chip has gone into a undefined state and I don't know how to reset it. I cannot reset the PWR module which contains the WKUP logic according the spec. The watchdog timer works and very reliable. I saw an ERRATA on this PA0 WKUP issue and it says clear the PA0 source before going to STANDBY. It is always cleared and I see good pulses on the PA0 on oscilloscope. I am using a jumper to connect the PA0 to 1.8V to wake the chip up. #pa0 #standby #stm32f4xx #wkup2016-11-21 7:50 AM
Hello,
Have you try the ready example under the STM32CubeF4 package?This firmware package contains a working example shows how to enter the system to STANDBY mode and wake-up using external RESET or WKUP pin. Hope this example can help you in your project to identify your issue: STM32Cube_FW_F4_V1.13.0\Projects\STM32469I-Discovery\Examples\PWR\PWR_STANDBYRegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.