STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f070 low power mode flash programming and DMA

Posted on October 25, 2016 at 08:18Dear All,I am new in stm32 world.The device I am going to make, its on low power mode.As far as I know from STM32F070xB /STM32F070x6 datasheet, it has 128KB flash memory.Now my question is 1.can the DMA request acc...

BSS and DATA size too big

Posted on November 22, 2016 at 01:38Hello I'm developing code for a STM32F031G6 on System Workbench. This microcontroller has 4KB of SRAM but after compiling my code (even with a empty main loop and nothing else declared) I get the following code si...

STM32L476VG - RTC - Vbat

Posted on September 14, 2016 at 19:08Dear Gents,I am using a STM32L476VG for my application. The RTC can be powered by Vbat provided by an external battery in case that VDD drops off. In this mode, when the MCU is powered by Vbat, only the RTC works...

mejrissi by Associate II
  • 2794 Views
  • 6 replies
  • 0 kudos

Slave/Master? Sm-Bus

Posted on November 21, 2016 at 13:54Hey, is it possible to use the I2C-SM-Bus-Modul as Slave or Master? I want use one I2C-Module as SM-Bus Slave and a other as Master.

communication using usart

Posted on November 14, 2016 at 06:43The original post was too long to process during our migration. Please click on the attachment to read the original post.

anjana087 by Associate II
  • 2436 Views
  • 3 replies
  • 0 kudos

14: error: expected declaration specifiers or '...' before

Posted on November 21, 2016 at 08:53i get 14: error: expected declaration specifiers or '...' before 'GPIO_Init'and its my source code :void Init_IO(GPIO_Init* GPIOx, uint32_t Pin, GPIOMode_TypeDef Mode, GPIOPuPd_TypeDef Pupd, GPIOSpeed_TypeDef Spee...

noval by Associate II
  • 1841 Views
  • 2 replies
  • 0 kudos

STM32F1 I2C1 Alt Functions Drive Low

Posted on November 16, 2016 at 02:39I am running into an issue with I2C on an STM32F103 that is driving me crazy.  The code worked on the same processor with the normal pin mapping, however on new hardware with the alternate pin mapping for I2C1 (Po...

drew by Associate III
  • 2262 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.