STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

fatfs create file in directory

Posted on December 14, 2016 at 14:07Hi,I am using fatfs sdcard stack, how can i create file in a directory? can i use f_open function for this? In f_open function i just specify the name of the file like this:f_open(&MyFile, 'STM32.TXT', FA_CREATE_A...

er3481 by Senior
  • 2725 Views
  • 1 replies
  • 0 kudos

Resolved! Stm32f4 DMA doesn't always restart after suspending

Posted on December 13, 2016 at 19:27I am trying to implement such an algorithm on Stm32f4-discovery: Initialize the DMA and Tripple-ADC in the interleaved mode on the same channelWait for an external interruptSuspend the DMA and ADCsSend the buffer...

STM32F401 problem RTC and debug SWD

Posted on December 11, 2016 at 13:34Hi!Immediately after reading the time from the RTC using HAL_RTC_GET_TIME RTC clock stops. Changes only position Subsecounds. The second problem is that when you first start debugging is successful but the stay an...

BlueNRG-1 Latency

Posted on December 14, 2016 at 10:53Hi,Please help me with the following theoretical situation: I have a BlueNRG-1 running HID profile, mostly sleeping. From time to time, an external interrupt occur (GPIO line) and the time interval in which the MC...

Timeout error trying to connect via ''external mode''

Posted on April 01, 2015 at 18:22Hi, I posted a question yesterday which was solved by myself about the external mode connection. But now I am getting another problem, a timeout error. I am using the ''Embedded Coder Support Package for STMicroelect...

Trouble Resetting Nucleo-F091

Posted on December 10, 2016 at 00:53Hi Everyone.I have a very strange problem with a Nucleo-F091RC board. I've been playing around with a serialprogram just to print messages via the uart, just to get the first project started. I noticed as long as ...

kvresto by Senior
  • 2035 Views
  • 9 replies
  • 0 kudos

Image to byte converter of STM

Posted on December 13, 2016 at 17:00Hi,I am interested with web server raw.I need converter image to byte array of ST.Where can I find that program?thanks.

ali2399 by Associate II
  • 1817 Views
  • 2 replies
  • 0 kudos

UM1734 - Issue with the ''Usage'' description?

Posted on December 13, 2016 at 21:59Is it just me or is the ''Usage'' stuff mostly upside down and backwards? Me - I'm tending to believe the README.  ------------------------------------------------UserTxBufferManual UM1734:README.TXT:- 1 x Bulk IN...

0690X00000605q6QAA.png 0690X00000605q2QAA.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.