STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Trying to set BOR threshold without success

Posted on December 14, 2016 at 23:55I am trying to write code to set the BOR Level under program control for the STM32L151 but cannot get the result I need. I have the following:if ((FLASH_GetUserOptionByte() & 0x0F) != OB_BOR_LEVEL4){      FLASH_Un...

arthurg by Associate II
  • 1164 Views
  • 1 replies
  • 0 kudos

STM32VLDISCOVERY board

Posted on December 14, 2016 at 08:44Hello Team,We are working on one project, and we are planning to use STM32F103RGT6 and STM32F205RGT6 MCU.but before that we are testing our application using STM32VLDISCOVERY board and this board is working good.N...

STMFlash Loader command line

Posted on December 15, 2016 at 03:39Hi, we use STM32F407. STMFlashLoader is V2.8.0. I use STMFlashLoader Demo.exe successfully if I set Boot0 to 1.For some reasons, I need to test the STMFlashLoader.exe using the command line to download the firmwar...

xin gao by Associate
  • 994 Views
  • 0 replies
  • 0 kudos

STM32L0Cube UART HAL pulls in extraneous floating point code

Posted on October 30, 2016 at 18:47Hi, The latest STM32L0Cube UART Hal pulls in unnecessary floating point code when initializing the UART. The culprit is the __DIV_LPUART macro, which contains a floating point number (256.0). When replaced with the...

tony2399 by Associate II
  • 1342 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L0 vs STM32F0 huge difference in base code size

Posted on December 11, 2016 at 11:25HI All,I am wondering why initial code size differs with a factor of 3 between the STM32F031K6 and the STM32L031K6 - just for making an LED blink.I use CubeMx to generate the project and GCC (OpenSTM32 AC6 IDE) to...

SysTick ISR not called under debugger

Posted on December 14, 2016 at 13:39 Hi all. I noticed that when debugging a STM32F091 MCU my systick ISR never gets called. I Use STMCube library, so HAL_GetTick and HAL_Delay ceases to work as well (because uwTick is not increased). But onl...

Problems with STMFlashLoader Demo

Posted on December 13, 2016 at 19:43I am using STMFlashLoader Demo v2.8.0I recently upgraded as I am bringing up a new board design that uses STM32F427. I am unsure if these issues exist in previous versions, but the first issue probably does.Issue ...

MDC Stream options, STM32F745IE ETH IP

Posted on December 14, 2016 at 20:22Referencing P 1484 RM0385, Table 247 (Rev 6 of this RM.)The table shows bits for the operation field to be 10 or 01. I'm wprking with an Ethernet PHY that has extended function registers which are addressed by set...

hbarta2 by Associate III
  • 675 Views
  • 0 replies
  • 0 kudos

C file not recognizing #define

Posted on December 09, 2016 at 13:36My IDE has a feature that uses less contrasting text for code that is 'inactive' (not included) from this I found that some code is not being included that i had expected to be. For instance stm32f0xx_ll_tim.c   &...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.