STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to receive UART fixed length datas in sequence

Posted on January 24, 2017 at 15:27Hi allI'd like to use UART to receive soe fixed length datas, ex.'1234567890'.uint8_t buff[10]; hal_uart_receive_it(&huart, buff, 10); or hal_uart_receive_dma(&huart, buff, 10);How should I do and then make sure th...

CubeMx dma spi:Getting spi overrun

Posted on January 24, 2017 at 14:39Hi,I'm using latest version of Cube (download 20.01). I'm trying to read ADC-values from SPI with DMA. Read is activated on ADC-dataready.#define ADC_BLOCK_SIZE 24uint8_t tempBuf[ADC_BLOCK_SIZE ];// This interrupt ...

teijo by Associate II
  • 1523 Views
  • 1 replies
  • 0 kudos

F4 Analog Watchdog run-time reconfiguration?

Posted on January 23, 2017 at 18:35As the title says, can the analog watchdog high and low thresholds on F4xx be reconfigured while the ADC is running?I vaguely recall reading somewhere that it could be changed dynamically at any time but can't for ...

parsec by Associate III
  • 1736 Views
  • 2 replies
  • 1 kudos

CubeMX FreeRTOS USB and USB_CoreInit function

Posted on January 20, 2017 at 17:05HiI used STM32CubeMX and configured a project using RTOS and USB_DEVICE (I am trying to run the USB CDC functionality with the FreeRTOS). The program runs until it hits the USB_CoreInit function inside stm32f4xx_ha...

STM32F103 - Use of PWM (Timer1) without the debugger

Posted on January 24, 2017 at 07:58Hi,We configure the timer 1 to run a PWM signal on PA8 & PA9.It works well with the debugger, but when we power the MCU directly, the PWM is not running ! (We can confirm that the main is running... with a manual G...

samuel23 by Associate III
  • 2174 Views
  • 4 replies
  • 0 kudos

Resolved! 32F413HDISCOVERY - HS USB?

Posted on January 23, 2017 at 23:01The 32F413HDISCOVERY  webpage, and also the data brief DocID029964 Rev 1, both say the kit has:USB OTG HS with Micro-AB connectorhowever, the STM32F413 has 'only' an USB OTG FS.Also, on the picture of the DISCO's P...

STM32F4 lwip dropping packets?

Posted on January 08, 2017 at 21:24Hello all,I'm currently working on a bridge that takes in artnet packets (theatrical lighting control) and spits it out as data for ws8212 leds.I've got working code setup and running on an olimex stm32-E407 dev bo...

SPI DMA RX, polled TX hardfaults in HAL

Posted on January 13, 2017 at 00:15I've run out of DMA channels so I can't run SPI2 with DMA both ways. Since I'm talking to an external NOR flash chip where reading data is of much higher priority than writing I'd be happy with RX only DMA.Setting ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.