STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L052 USB communication problems

Posted on January 24, 2017 at 11:58Hi,I'm running in some communication problems with USB at the STM32L052 on Linux. If the device is connected via /dev/ttyACM0 and transmitting data to the host, I see an echo on the receive buffer inside the STM. I...

skamlah by Associate
  • 1513 Views
  • 3 replies
  • 0 kudos

What is nRSTIN pin?

Posted on January 26, 2017 at 01:55I have 'Getting started with STM32F4xxxx MCU hardware development' pdf. It is from December 2016, probably the newest. In page 30/40 Table 8 there are 5 pins needed for programming? Five pins. But on the next page ...

LMI2 by Lead
  • 1700 Views
  • 4 replies
  • 0 kudos

STM32L431 - UID readable via Bootloader?

Posted on January 26, 2017 at 12:04Hi,can you read the UID of the mentioned processor bny means of the bootloader? Reading AN2606, Table 106 it seems that the UID is out of reeadable range. Maybe somebody could confirm?Regards

ulf2 by Associate
  • 655 Views
  • 0 replies
  • 0 kudos

adc multiple value without dma

Posted on January 26, 2017 at 08:35Hi all,I try to read ADC values from the STM32f303 without success. With one channel everything is working fine but when I want to read the next channel it is not working any more. maybe I am doing something wrong ...

Hall sensors not triggering IRQ from TIMER2

Posted on January 02, 2017 at 18:14Hello,i am working on a bldc motor project for school, and for start to understand whats happening inside the IRQ handler, i have configured timer2  on ch1,2,3 with 3 emulated hardware signals, imitating the CW of ...

0690X00000605yKQAQ.png
Bogdan by Senior
  • 3141 Views
  • 10 replies
  • 0 kudos

Resolved! F1 RTC prescaler

Posted on January 25, 2017 at 15:54Hello,while rm0008 Rev. 16 18.4.3 says:Note: If the input clock frequency (fRTCCLK) is 32.768 kHz, write 7FFFh in this register to get a signal period of 1 second.STM32Cube_FW_F1_V1.4.0/Drivers/STM32F1xx_HAL_Driver...

STM32L053 NUCLEO64 issues

Posted on January 26, 2017 at 10:06Hello all. I have a STM32L053 NUCLEO64 (my third one now) and it has blown again. I can't figure out where I am going wrong. I am powering via the USB from my PC. The common theme seems to be that it happens when I...

ADC triger on PWM edge

Posted on January 25, 2017 at 22:27Hello,On a STM32F407VE device   i have a timer2 which reads 3 hall sensors from a bldc motor,  this timer is feeding the trigger signal into a advanced timer1 which generates 6pwm's for the transistor bridge.The  r...

Bogdan by Senior
  • 1479 Views
  • 2 replies
  • 0 kudos

stm32f103ret6 internal temperature sensor range

Posted on January 25, 2017 at 02:01Hi,I am using STM32F103RET6 as microcontrller.   In ADC1, there is a internal temperature sensor.  Can this sensor read up to 150C, what is the temperature reading range of this sensor?Thanks, Jian#temerature-senso...

Jian Chen by Associate II
  • 2396 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.