2017-01-25 11:35 PM
Hi all,
I try to read ADC values from the STM32f303 without success. With one channel everything is working fine but when I want to read the next channel it is not working any more. maybe I am doing something wrong with the GetConversionValue(ADC1) ? I want to save here up to eight values. Thanks for your input. Here is the code:
/* Configure the ADC clock */
RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div2);/* Enable ADC1 clock */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_ADC12, ENABLE);/* Setup SysTick Timer for 1 �sec interrupts */
if (SysTick_Config(SystemCoreClock / 10000)) { /* Capture error */ while (1) {} }/* ADC Channel configuration */
/* GPIOC Periph clock enable */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE);/* Configure ADC Channel7 as analog input */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 ; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(GPIOC, &GPIO_InitStructure); ADC_StructInit(&ADC_InitStructure);/* Calibration procedure */
ADC_VoltageRegulatorCmd(ADC1, ENABLE);/* Insert delay equal to 10 �s */
// Delay(10);ADC_SelectCalibrationMode(ADC1, ADC_CalibrationMode_Single);
ADC_StartCalibration(ADC1);while(ADC_GetCalibrationStatus(ADC1) != RESET );
calibration_value = ADC_GetCalibrationValue(ADC1);ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_CommonInitStructure.ADC_Clock = ADC_Clock_AsynClkMode; ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled; ADC_CommonInitStructure.ADC_DMAMode = ADC_DMAMode_OneShot; ADC_CommonInitStructure.ADC_TwoSamplingDelay = 9;ADC_CommonInit(ADC1, &ADC_CommonInitStructure);
ADC_InitStructure.ADC_ContinuousConvMode = ADC_ContinuousConvMode_Enable;
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; ADC_InitStructure.ADC_ExternalTrigConvEvent = ADC_ExternalTrigConvEvent_0; ADC_InitStructure.ADC_ExternalTrigEventEdge = ADC_ExternalTrigEventEdge_None; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_OverrunMode = ADC_OverrunMode_Disable; ADC_InitStructure.ADC_AutoInjMode = ADC_AutoInjec_Disable; ADC_InitStructure.ADC_NbrOfRegChannel = 2; ADC_Init(ADC1, &ADC_InitStructure);/* ADC1 regular channel6 configuration */
ADC_RegularChannelConfig(ADC1, ADC_Channel_6, 1, ADC_SampleTime_19Cycles5); ADC_RegularChannelConfig(ADC1, ADC_Channel_7, 2, ADC_SampleTime_19Cycles5);/* Enable ADC1 */
ADC_Cmd(ADC1, ENABLE);/* wait for ADRDY */
while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_RDY));/* Start ADC1 Software Conversion */
ADC_StartConversion(ADC1);/* Infinite loop */
while (1) { /* Test EOC flag */ while(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET);/* Get ADC1 converted data */
ADC1ConvertedValue =ADC_GetConversionValue(ADC1);/* Compute the voltage */
ADC1ConvertedVoltage = (ADC1ConvertedValue *3000)/0xFFF; }}#adc-multiple-value-without-dma2017-01-26 2:50 AM
Hello Werner
I have moved your question to the
‌ where someone should be able to assist you.Thanks
Oli
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.