STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

spi transmit without mcu control

Posted on January 20, 2017 at 06:22I'm learing stm32 spi,In normal way of master mode, I have to low the slave select pin, then transmit data, then high the slave select pinI know that I can use dma to transmit data,but I am not sure that dma can co...

ctc.ctc by Associate II
  • 2346 Views
  • 4 replies
  • 0 kudos

Interface 5 motors requiring n-Pulse Generation mode

Posted on January 24, 2017 at 22:25I asked a question earlier on how to generate n-Pulses from STM32 to drive a servo like interface -> https://community.st.com/0D50X00009XkdsSSAR, and it worked. This feature is available only on TIM1/8. Is there a ...

Neo M by Associate II
  • 4480 Views
  • 11 replies
  • 0 kudos

CAN interface stack for STM32F0 series controllers

Posted on January 24, 2017 at 18:54I am building a peripheral device that will use an STM32 microcontroller.  This peripheral device will communicate with a master/supervisory device over a CAN interface.  We have tentatively chosen the STM32F091CC ...

ADC values reading with DMA

Posted on January 21, 2017 at 07:17The original post was too long to process during our migration. Please click on the attachment to read the original post.

brent Kim by Associate II
  • 3899 Views
  • 5 replies
  • 0 kudos

STM32F303K8 timer interrupt hangs

Posted on January 25, 2017 at 11:07Hi,I try to implement a timer with interrupt routine, but it always hangs after the timer is activated. This can be seen if I use the debugger over SWD: when I execute the next command after TIM_Cmd(TIM2, ENABLE); ...

4tschabos by Associate II
  • 2109 Views
  • 5 replies
  • 0 kudos

UART2 can't receive data from PC in STM32L476RG nucleo

Posted on January 24, 2017 at 11:54Hi allI'd like to use UART2 to receive data, but It seemed to be failed, only could transmitted data.I used the same codes in UART1, everything is fine,So I think HW and SW parts are fine except UART2.I had not con...

0690X00000605zpQAA.png

Resolved! STM32F4 GPIO functions

Posted on January 24, 2017 at 15:09I have looked at PM0214 Programming manual for STM32F4 series for functions like GPIO_Write() and GPIO_ToggleBits() but they don't seem to be there. Is there a document that describes peripheral functions or does o...

John Hite by Associate III
  • 1705 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.