STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U575 SMPS time out when enabling. What to check for?

My controller uses the STM32U575 chip. I followed the recommended design for the SMPS using the same inductor and XR7 capacitors as recommended in the reference design. I built up 4 boards, the first three boards worked properly without issue. After ...

ScottD by Associate II
  • 2884 Views
  • 7 replies
  • 1 kudos

fail to write on sd card on stm32 g491re

Hi all,i am currently writing a program which is supposed to write data on an sd-card. This has worked until i changed my laptop (and cubeIDE version from 1.13 to 1.17) and until i added line 127 "HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_SET);"....

jan212 by Associate
  • 1426 Views
  • 2 replies
  • 0 kudos

Using Hex file or Bin file for FOTA?

Hi community!I've been tasked with designing and programming a new product that includes a bootloader and LTE communication, the main issue I'm facing now is to design the whole updating and downloading process, supposedly I'll store the update in a ...

Resolved! stm32f4xx hal systick question

in stm32f4xx_hal.c file the function __weak HAL_StatusTypeDef HAL_InitTick uses a function HAL_SYSTICK_Config thats in stm32f4xx_hal_cortex.c file and that function uses SysTick_Config(TicksNumb) but i cant find this function .just wondering where th...

Failed to inerface (4 and 8 GB) pendrive to STM32H747

 Dear Community, I am currently working on interfacing of USB (pen-drive) in FS mode with STM32H747BIT6.I have observed that  during the enumeration process of pen-drive it is failing  to proceed at the functionUSBH_HandleControl --> case CTRL_SETUP_...

Rushali by Associate III
  • 2408 Views
  • 4 replies
  • 4 kudos

LPTIM behaviour

Hallo, I'd like to use LPTIM to count the number of digital impulse of a signal.So, the signal is connected to (in this case) LPTIM2_IN1.The init function (MX_LPTIM2_Init) is as this: hlptim2.Instance = LPTIM2; hlptim2.Init.Clock.Source = LPTIM_CLOCK...

IVent.1 by Senior
  • 871 Views
  • 1 replies
  • 0 kudos

Resolved! [STM32H7] CORTEX_M7 configuration for MPU in CUBEMX

Dear Experts,I am looking at configuring the CORTEX_M7 section for my custom STM32H743VIT6 based board. Below are the functionalities that I plan to use with the board:a. Sensors' reading via SPI, I2C, b. Communication via UART/USART, USB, Ethernet (...

KhangRtR by Associate II
  • 3690 Views
  • 5 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.