STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Buck converter with peak current mode -Sawtooth generator

Hii, I'm new to embedded systems. I have the B-G474E-DPOW Discovery kit with STM32G474RE MCU and I implemented the peak current mode Buck converter(HW) as described in the application note of stm. The only thing that I cannot understand is how exactl...

Fani by Associate
  • 1509 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H5 Interface With Gigabit Ethernet PHY device

Moved from MPUs forum.Hi, i must Use a Single Port Gigabit Ethernet PHY  that have a RGMII Gigabit Interface to connect a RMII 10/100 MbitEthernet MAC interface of the STM32H563VI MCU. Do you think it is possible to connect a Gigabit PHY chip to the ...

B.Michele by Associate III
  • 7002 Views
  • 10 replies
  • 3 kudos

Wrong echo from STM32F4 USB device

Hi all,I'm developing a composite USB device on USB OTG port on a board based on STM32F429 chip.The device has two interfaces: a custom device + a CDC device. I'm using USB_Device_Library code.Windows host correctly shows 3 items: the composite devic...

SteMMo by Senior
  • 5023 Views
  • 7 replies
  • 1 kudos

Resolved! STM32U575RGT6 without UCPD

Hi,We're in the process of developing a new board and I've got a question about USB.We would like to have a USB device with MSC only.Can we not activate the UCPD and work with the TCPP01-M12 FLT, DB CC1 and CC2 signals at ground (as on the STM32U545 ...

Resolved! STM32U575RITxQ SPI 3 fails at 1024 bytes or more

Hi, this is new for me. im working with a project that includes an STM32U575RIT6Q controlling a device through the SPI3 interface at 40MHz with 8 bits per word, SPI mode 0, and the GPIO change speed at very high. The microcontroller is running at 160...

cesarv by Associate II
  • 2032 Views
  • 2 replies
  • 1 kudos

STM32F411RE as ISO7816 Slave mode (card emulation)

Hello,I’m trying to use an STM32F411RE microcontroller as an ISO7816 smartcard slave rather than a reader (i.e., to emulate an actual smartcard). In this scenario, the clock would come from an external source, and the MCU would respond with an ATR an...

cucabelu by Associate
  • 1908 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.