2025-02-04 7:44 AM
Hi,
We're in the process of developing a new board and I've got a question about USB.
We would like to have a USB device with MSC only.
Can we not activate the UCPD and work with the TCPP01-M12 FLT, DB CC1 and CC2 signals at ground (as on the STM32U545 eval kit)?
At the moment, I can't get the USB to work without the UCPD enabled on the NUCLEO-U575ZI-Q board.
Solved! Go to Solution.
2025-02-12 6:52 AM
Hello,
I could not get the USB device to work without the TCPP01-M12 FLT, DB CC1 and CC2 signals.
I have modified my hardware to drive the signals as on the NUCLEO-U575ZI-Q board.
thank you for your feedback.
2025-02-04 11:17 PM - edited 2025-02-04 11:19 PM
Your question:
We would like to have a USB device with MSC only.
Can we not activate the UCPD and work with the TCPP01-M12 FLT, DB CC1 and CC2 signals at ground (as on the STM32U545 eval kit)?
I think it is OK to have a USB device with MSC to work without UCPD (UCPD pins floating).
2025-02-12 6:52 AM
Hello,
I could not get the USB device to work without the TCPP01-M12 FLT, DB CC1 and CC2 signals.
I have modified my hardware to drive the signals as on the NUCLEO-U575ZI-Q board.
thank you for your feedback.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.