2025-02-07 2:45 AM - last edited on 2025-02-07 2:50 AM by Andrew Neil
Moved from MPUs forum.
Hi, i must Use a Single Port Gigabit Ethernet PHY that have a RGMII Gigabit Interface to connect a RMII 10/100 Mbit
Ethernet MAC interface of the STM32H563VI MCU.
Do you think it is possible to connect a Gigabit PHY chip to the 100 Mbit H5 micros??? pin out,
Sure the final Ethernet Speed of the system, will be declasses to 10/100 Mbit.
In particular I can't find where to connect the PA7 pin [RMII_CRS_DV] Carrier Sense... there is no CRS_DV output in the PHY gigabit device
Thank you very much
Solved! Go to Solution.
2025-02-13 1:15 AM
Ok thank you,
we are also just looking for a newer chip than the LAN 8742, we will probably choose the Microchip or TI brand
2025-02-07 3:57 AM - edited 2025-02-07 3:58 AM
Hello,
STM32 MCUs don't support Ethernet Gigabit. Only MPU family does: STM32MP1xx, STM32MP2xx
2025-02-07 6:31 AM
Not possible to connect RGMII PHY to an RMII interface. They are using different signals and clocks.
You need to look for a RMII PHY.
Regards.
2025-02-07 7:11 AM
Good evening SofLit,
Thank you for your answer; Yes I Know that STM32H563VI MCU haven't the Gigabit Interface but only the 10/100 Mbit/s Fast Ethernet Like All H5-H7 ecc.. STM Arm processor
For me it' Ok to have only 100 Mbit/s speed But I want Interface the PHY Phisical Layer to magnetic and RJ45 Copper Ethernet line With a New Chip Gigabit that have RGMII line.
So i want interface the RMII or MII Interface of STM H5 With a RGMII PHY Chip;
Is it possible to adapt the signals together with some I/O pins to drive the RGMII interface by downgrading it to max 100 Mbit??
Thank's
2025-02-07 8:05 AM
Good evening PatrickF,
Thank you for your answer; Ok The H5 MCU haven't the RGMII but only the SMI, MII, RMII, interface.
I was wondering if it's not really possible to adapt the signals together with some I/O pins to drive the RGMII interface by downgrading it to max 100 Mbit?? with the RMII Or MII H5 pinout and some other I/O pin....
downgrading the clock to 25 MHz I think, or whatever it takes....
Thank's
2025-02-07 8:27 AM
Hi, @B.Michele
sorry to be rude, but I fear there is no way, they are too different.
RGMII PHY could run on 100Mbit/s link, but it is still using RGMII protocol.
Either you use an RMII PHY with STM32H5, or use an STM32 having RGMII capabilities (STM32N6, STM32MP1, STM32MP2 families).
Regards.
2025-02-07 1:02 PM - edited 2025-02-07 1:03 PM
@B.Michele Please ask the vendor of the PHY if they support RMII. We have successfully connected STM32H753 to a 10/100/GB Broadcom switch chip, in 100 M RMII mode.
2025-02-10 12:08 AM - edited 2025-02-17 1:32 AM
Thank you @PatrickF
Ok, thanks for the advice, so ultimately the "Copper" or "Fiber" Ethernet PHY device must support one of the two protocols of the H5: 'MII' or 'RMII'
The H5 MCU have only the MII and RMII Media Independent Interface that i must use. Together with the SMI serial signal realize the MAC interface for the PHY device.
-----
So the last question for reflection is that with a RMII MAC and a PHY that supports both copper and fiber I can achieve 100 Mbps with both magnetic and RJ45 and optical fiber?? with only RMII protocol ??
Thank's @PatrickF
2025-02-10 12:21 AM - edited 2025-02-11 12:35 AM
Thank you @Pavel A.,
Thanks for your suggestion, certainly i see the opinion too with my MaxLinear Single Port Gigabit Ethernet PHY with RGMII Or SGMII interface. H7 & H5 I think they have the same Ethernet MAC interface.
I can only ask you the brand of the PHY chips ??
Thank's
2025-02-12 2:12 PM
> I can only ask you the brand of the PHY chips
For bring-up we used PHYs similar to LAN8742.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.