STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

GPIO ODR Register

Posted on July 09, 2017 at 20:32Hello, Was doing some tests with the ODR register for GPIO and noticed that when I load it with 0xFFFF some pins (13-15 for GPIOA &GPIOC) were still off. I have them initialized so I am unsure why they won't come on. ...

STMF100RB Encoder Interface

Posted on July 10, 2017 at 03:16Hello,I have set up an encoder interface using SPL stm32f10x_tim.h which blinks an LED every time the motor makes a revolution. I am wondering how I would go about getting direction data from a similar setup. &sharpin...

stm32f373 SDADC doesnt work when USB starts

Posted on July 06, 2017 at 09:43I'm using STM32F3xx USB full speed device library (UM0424), it works well. And I need SDADC in my project. So I wrote simple test:start conversion in SysTick every 100msvoid SysTick_Handler(void){if(adc_ready)    {  ...

reciver remote with stm32

Posted on July 09, 2017 at 07:48hi my friends ineed some help i wana creat a project with stm32 to learn remote(pt2262),i need program with explain plz help me

why does my linear sensor array not scale/normalize?

Posted on June 30, 2017 at 15:57I'm using STM Studio to tune my linrot (linear) sensors according to this application note:'AN4316 Application note Tuning a STMTouch-based application'I did this before and it appeared to work.  However with this new...

RM0390 STM32F446xx Reference Manual update request

Posted on July 09, 2017 at 16:27In RM0390, the Reference Manual for STM32F446xx MCUs, on page 379, Section 13.10 Temperature sensorThe formula given isTempC = ((Vsense - V25) / Avg_Slope) + 25In the STM32F446xC/E Data Sheet, page 147, Section 6.3.22...

Resolved! Error in Alternate Functions on STM32F030?

Posted on July 08, 2017 at 22:35On page 34 of the STM32F030 datasheet there is a table of Alternate Functions that I think contains an error.If you look at the GPIOA_AFR registers for port A and select column AF4 you will see that TIM14_CH1 is menti...

Willunen by Associate III
  • 2556 Views
  • 3 replies
  • 0 kudos

RTC GET_Time Help

Posted on June 08, 2017 at 18:14 Plese . I have some problems with RTC Calendar. I do not understand how to use it. You can send me some examples for STM32f407VGTx Discovery. (HAL Library)With HAL_RTC_SetTime (& hrtc, & sTime,...

Dynamic Change Duty Cycle PWM using tim.h

Posted on July 04, 2017 at 22:53Working off the provided example for PWM on STM32F100RB I am able to output varying levels of PWM, however, my attempts to change the duty cycle of a specific channel according to user input have failed. I do not see ...

STM32F100RB PWM Input Capture

Posted on July 08, 2017 at 23:04Attempts to capture external PWM signal with TIM.h library have been unsuccessful. I figured using semihosting to print values to console would be helpful in debugging however the values refuse to change although I kn...

0690X00000607TJQAY.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.