2017-07-04 1:53 PM
Working off the provided example for PWM on STM32F100RB I am able to output varying levels of PWM, however, my attempts to change the duty cycle of a specific channel according to user input have failed. I do not see any way to change the duty cycle using tim.h except on timer initialization.
#duty-cycle #pwm #dynamic-change2017-07-05 1:45 AM
It would have been nice to have more information about what you are using e.g. STM32Cube, the standard perihperal libray or whatever.
However to change the duty cycle you just have to modify the autoreload and compare register on the fly. If PWM is running, then stop it. Afterwards modify the registers and start it again. If you use STM32Cube there should be __HAL_TIM_SET_AUTORELOAD and __HAL_TIM_SET_COMPARE to do the job.
2017-07-05 5:54 AM
tim.h? where'd you get that?
TIMx->CCRx = Width;
Where Period = N-1, Width = N/2 is 50% duty
2017-07-05 4:37 PM
I have been using Coocox and it lets me enable the timer library:
#include <stm32f10x_tim.h>
I am not familiar with how to do this by writing to the registers or using HAL, if you think these methods are easier I could use some help getting my foot in the door. I figured these libraries and documentation would be my best bet to learn fast but I could've been mislead.
2017-07-08 5:15 PM
Ok, so the SPL (Standard Peripheral Library), I'm good with that.
The register in this case is simple enough, the library works well for initialization, but when you're just wrapping a register write sometimes it makes sense to just do that.
/**
* @brief Sets the TIMx Capture Compare1 Register value * @param TIMx: where x can be 1 to 14 except 6 and 7, to select the TIM peripheral. * @param Compare1: specifies the Capture Compare1 register new value. * @retval None */void TIM_SetCompare1(TIM_TypeDef* TIMx, uint32_t Compare1){ /* Check the parameters */ assert_param(IS_TIM_LIST1_PERIPH(TIMx));/* Set the Capture Compare1 Register value */
TIMx->CCR1 = Compare1;}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.