STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Build a project with a single button.

Posted on July 08, 2017 at 00:39I continue to look for answers to difficult questions.There is a project for an arm under GCC with a static load. Addresses of variables and data do not change, for gcc everything is known, and it successfully optimiz...

Receive CAN msg in interrupt mode with STM32F105 mcu

Posted on July 07, 2017 at 19:40Hi everyone,I'm trying to receive a msg via CAN-bus in interrupt mode with STM32F105 mcu. I set the CAN filter so that only 0x0106 and 0x010A IDs are allowed. This is the first time I use this microcontroller so I'm n...

SPI CPOL takes effect only after SPE is set

Posted on July 04, 2017 at 05:25I understand that CPOL takes effect only after SPE is set. But when I talks with AD7606, I need to have CPOL high at idle, and one line only(either BIDIMODE=0 or BIDIMODE=1) for receiving. In this mode, SPE can only b...

T YX by Associate
  • 1549 Views
  • 2 replies
  • 0 kudos

SPI in Master Mode with NSS Hard Output

Posted on July 07, 2017 at 20:42Hello, I interfaced STM3210E-EVAL with external RF Slave chip and trying to place a data in a slave register.Ex data: Slave register address is 0xC0 and placing two bytes of data (0x00 and 0x12). For this I  configure...

0690X00000603vxQAA.jpg
suresh by Associate II
  • 1554 Views
  • 2 replies
  • 0 kudos

problem about LSE clock of stm32l431

Posted on March 15, 2017 at 07:30hi,I want use LPTIM1 and select clock source is LSE.when i enable LSE use code auto-gen from stm32cubemx,but LSERDY can't assert,the external OSC is work normal.init code like as:void SystemClock_Config(void){  RCC_O...

cai.bai by Associate II
  • 2414 Views
  • 4 replies
  • 0 kudos

Resolved! DFSDM limited dynamic range at high F_OSR?

Posted on July 07, 2017 at 05:45For a while now, I've been wanting to learn the DFSDM (cascaded-integrator-comb, or CIC, filter) peripheral on the STM32L4 and use it for some serious DSP work.  This week I finally had time to dig in and get it worki...

mhaun by Associate II
  • 3153 Views
  • 2 replies
  • 0 kudos

ULPI read registers

Posted on July 07, 2017 at 14:43Hi, could you help me please to implement reading registers from USB ULPI chip ?thanks for all repliesKind regards ...

STM32CubeF4 fail clock configuration FreeRTOS projects.

Posted on July 07, 2017 at 19:35I'm trying to implement a FreeRTOS program on an STM32F429I-Disco (first rev.) using the examples in STM32CubeF4 (V1.16.0). Neither the 'Demonstration' project not the 'FreeRTOS_ThreadCreation' project will run. They ...

[Windows 10 x64] CubeMX updater deleted executable

Posted on March 20, 2017 at 08:40I tried to update STM32CubeMX yesterday to V4.20 using the built in updater (via Check Update Manager). After files were downloaded the update process started normally. Right after installation appeared to have compl...

parsec by Associate III
  • 2913 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.