2025-02-18 1:45 AM
Hi I am using STM32F407 DISCOVERY BOARD and I am able to make the board change to boot mode using a another controller.
After boot mode change over I need to program the memory of STM32F407 DISCOVERY BOARD by UART communication.
Here I am unable to get the ack when I provide the sync command(0x7f).
But when I completely remove the power and provide the power back The 0x7f is acknowledged with 0x79.
In real time application I cannot reset the power manually.
Am i missing anything ...? Please share your insights on this.
2025-02-18 2:03 AM
> I am able to make the board change to boot mode using a another controller.
How?
JW
2025-02-18 5:48 AM
If ACK isn't being sent, it doesn't sound like you're in the bootloader. Unless another interface is active first.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.