STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB dual host application's problems by STM32F205

Posted on August 07, 2017 at 02:46Can I use dual USB host by ST's MCU(STM32F205RE)? Will it supported two USB interface to make two FS host controller (one is FS, another is HS and didn't use external phy)? have one have any suggestions about this? ...

david wu by Associate
  • 1105 Views
  • 1 replies
  • 0 kudos

[CubeMX Request] Move init functions from main.c

Posted on August 10, 2017 at 09:36As title says, this a request to move generated functions SystemClock_Config and LL_Init (when LL is used) from main.c to peripheral file, if 'Generate peripheral initialization as a pair of '.c/.h' files per periph...

George.P by Associate III
  • 1998 Views
  • 3 replies
  • 0 kudos

I2c cannot read from sensor

Posted on August 03, 2017 at 06:49 I am using mlx90614 sensor attached to my nucleo F091RC. I have a working code with mbed : double mlx90614::read_temp(uint8_t reg) { char cmd[2]; cmd[0] = 0x01; cmd[1] = 0x00; // Send start bit __i...

STM32F0 Discovery Flash Download Error!

Posted on August 10, 2017 at 10:39Hello to everyone. I am using Stm32f0 discovery (ST-Link) for the programmer. I will load the to external processor (STM32L011D3P6). I edited the Flash settings in Keil IDE. I get this error:'' Debugger - Cortex M E...

0690X00000607l9QAA.png

STM32F0 SPI transmit via interrupt

Posted on August 09, 2017 at 11:30Hello everyone,I'm useing the NUCLEO-F072RB and I'm trying to get the SPI via interrupts to work.Here is the CubeMX initialization of the SPI:/* SPI1 init function */void MX_SPI1_Init(void){      hspi1.Instance = SP...

PaKi by Associate II
  • 1488 Views
  • 2 replies
  • 0 kudos

Question about behaviour of HAL_UART_Transmit_IT

Posted on August 09, 2017 at 17:42Hello everyone,I am having some trouble understanding the behaviour of the HAL_UART_Transmit_IT and HAL_UART_Receive_IT routines. I am using two NUCLEO-F767ZI boards that communicate via UART1 in a request/reply fas...

Resolved! STM32F405: Unable to program

Posted on July 17, 2017 at 16:07Hi guys, I've been working with my STM32F405 for over a month now and all of a sudden my chip is unable to be programmed. When I attempt to program my chip using SW4STM32 I get this following error:    Open On-Chip De...

STM32F410-nucleo interval timer

Posted on August 10, 2017 at 05:12I am trying to code interval timer for stm32f410 nucleo demo board.Following is the code wherein I try to set the on-board LED-2 GPIO_PIN_5 as indication but till now no successPlease following is the code ....need ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.