2017-08-09 2:30 AM
Hello everyone,
I'm useing the NUCLEO-F072RB and I'm trying to get the SPI via interrupts to work.
Here is the CubeMX initialization of the SPI:
/* SPI1 init function */
void MX_SPI1_Init(void){hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER; hspi1.Init.Direction = SPI_DIRECTION_2LINES;hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_HARD_INPUT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 7;
hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}
In my main I start sending 3 bytes every 10 seconds by calling:
if (!(HAL_GetTick() % 10000))
{ u8_spi_tx_buffer[0] = 0xaa;u8_spi_tx_buffer[1] = 0x00;
u8_spi_tx_buffer[2] = 0xff;
if(HAL_SPI_Transmit_IT(&hspi1,u8_spi_tx_buffer,3) != HAL_OK)
{
/* Transfer error in transmission process */
Error_Handler();
}}
The 3 bytes are getting transmitted. However after about 30�s they are getting transmitted again. This happens about 20 times before they are getting stopped transmitting.
Do I have to do anything in the HAL_SPI_TxCpltCallback function to prevent this?
#stm32f0 #spi #stm32-spi-interrupts2017-08-09 4:02 AM
I was so focused on the initialization of the SPI thinking there has to be something wrong, that i didn't see the mistake is actually '
if (!(HAL_GetTick() % 10000))'...
Better going for a break and clean my mind...
2017-08-10 6:40 AM
I would do the following:
/* Declare two variables or two bits volatile */
volatile uint8_t SPIsending, NeedToSendSPI = false;
if (!(HAL_GetTick() % 10000))
{
if(!SPIsending)
NeedToSendSPI = true;
}
if(NeedToSendSPI)
{/* Will try recursively until SPI sending is accepted */
u8_spi_tx_buffer[0] = 0xaa;u8_spi_tx_buffer[1] = 0x00;
u8_spi_tx_buffer[2] = 0xff;
if(HAL_SPI_Transmit_IT(&hspi1,u8_spi_tx_buffer,3) == HAL_OK)
{
SPIsending = true;
NeedToSendSPI = false;
}
else
{
/* Transfer error in transmission process */
Error_Handler();
/* Deinit, Init, etc processes here */
}
}void HAL_SPI_TxCpltCallback(void)
{
SPIsending = false;
/* 1-2 ms to prevent sending again */
HAL_Delay(2); /* 1-2 ms to prevent sending again from 'if (!(HAL_GetTick() % 10000))' */
Do_WhateverAfter();
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.