STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103 ADC INTERRUPT from timer 1 CC1 doesn't start with HAL_ADC_START_IT().Adding HAL_ADC_START() after HAL_ADC_START_IT() Solves the problem. Why?

Posted on August 11, 2017 at 14:55I don't see the EOC interrupt stepping into action when using only START_IT().Using MXCube, attached is my user code.Haven't modified any header files. only the weak callback functions which are in my code.

Chen BH by Associate
  • 983 Views
  • 1 replies
  • 0 kudos

SD Card failing 'disk_initialize' in standalone mode

Posted on August 11, 2017 at 03:25I have an ST STM32F405 microprocessor. I generated my IAR Embedded Workbench 7.4 files using STM32 Cube software.  I'm trying to use the SD card resources to access a micro SD card on our custom board. When I use th...

Eric P by Associate
  • 1063 Views
  • 1 replies
  • 0 kudos

stm 32f 103 cubmx dma

Posted on August 11, 2017 at 14:36i need help for start used cubmx enable dma for read from spi 1 and write on spi 2if any one can help to me for fined reference document and examplethanks

STM32L1 internal temperature

Posted on August 09, 2017 at 14:44Hello,I use a STM32L151RCT6 on a custom board and i want to read the internal temperature. In the cube library I found an exemple using the LL library so I included the ll_adc driver in my code and tried to use it.W...

Resolved! Flash layout of an STM32F469IEH with 512kB Flash?

Posted on June 19, 2017 at 12:01Hi,we want to use the STM32F469IEH controller which has 512kB of Flash Memory. The Reference Manual does not show any Flash Layout of the 512kB Flash. I assume that it has the Layout of the 1MB Flash Memory with 1x512...

andi z by Associate II
  • 2160 Views
  • 4 replies
  • 0 kudos

Resolved! STM32CUBEMX

Posted on August 10, 2017 at 15:35Hi,Does the STM32CUBEMX support STM32L072KZ or any other MCU from STM32L0x2  series that has 128k of flash?I didnt find those MCU's...thanks...

kobi nis by Associate
  • 1496 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.