STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Failed to erase memory on Nucleo-FR446RE

Hello, A small disclaimer before beginning, this is my very first project on STM32, and my experience (currently being a student) with embedded systems as a whole is quite limited, so if I omit any important information, please indicate it for me. I'...

Capture d'écran 2025-02-19 173333.png Capture d'écran 2025-02-19 173518.png Capture d'écran 2025-02-19 174553.png
Edzzio by Associate II
  • 3630 Views
  • 8 replies
  • 3 kudos

[STM32H743VITx] PWM Configuration

Dear Experts, I am expecting to configure the PB5 of the STM32H743VITx as a PWM signal in order to trigger some external devices : I would like to generate a less-than 30Hz/60Hz pulse with variable duty cycle. Could you help or share some examples in...

Screenshot from 2025-02-20 11-17-02.png
KhangRtR by Associate II
  • 959 Views
  • 1 replies
  • 1 kudos

Resolved! STM32H743 external loader

I went through the ST External QSPI Loader how to and have verified my quadspi.c/h driver is good with the Winbond W25Q64 flash part we are using.  However after I create the .stldr and load it into the STM32 Programmer it will not read from the flas...

PFlor.2 by Senior II
  • 14595 Views
  • 21 replies
  • 2 kudos

Resolved! Dual bank boot up from bank2 is not saved in STM32F427VG

Hello, I am working on a product with dual banks enabled. In each banks, there are one bootloader and application. In bank1's bootloader, if new application arrived, it will update bank2's application and then reset and boot from bank2. I meet a prob...

melfice by Associate III
  • 1667 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L151RET6 Stop Mode and reset by watchdog

STM32L151RET6Is the RTC affected by the microcontroller reset?The system is placed in stop mode and is reset every 2 seconds by the watchdog.After 24 hours of operation, I find a delay of approximately 20 seconds.If I do not use stop mode and let the...

costi by Associate III
  • 2049 Views
  • 4 replies
  • 0 kudos

Resolved! STM32H735IGK6 SRAM and Flash Speed

Hello,i am wondering why i can't find any information how fast the different SRAMs are.For Flash you have to configure waitstates, to setup the speed according to the CLK, but not for SRAM.I guess, because there is a dCache installed, the SRAM does n...

AZorn.1 by Associate III
  • 1549 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.