2025-02-10 11:30 PM
Hello,
I am working on a product with dual banks enabled. In each banks, there are one bootloader and application. In bank1's bootloader, if new application arrived, it will update bank2's application and then reset and boot from bank2.
I meet a problem that the boot from bank 2 is not saved after power off. The code always boot from bank 1, after it lost power. In design, it should boot from the same bank as previous, while there is no firmware update.
Attached my code for setting OB_BFB2_ENABLE after firmware upgrade.
Thank you for assistances.
Melfice
Solved! Go to Solution.
2025-02-19 10:55 PM
For records, I have managed to implement the dual bank code.
{
FLASH_OBProgramInitTypeDef OBInit;
FLASH_AdvOBProgramInitTypeDef AdvOBInit;
HAL_FLASH_Unlock();
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPERR);
HAL_FLASH_OB_Unlock();
HAL_FLASHEx_OBGetConfig(&OBInit);
OBInit.OptionType = OPTIONBYTE_USER;
HAL_FLASHEx_AdvOBGetConfig(&AdvOBInit);
AdvOBInit.OptionType = OPTIONBYTE_BOOTCONFIG;
if ((AdvOBInit.BootConfig &OB_DUAL_BOOT_ENABLE)==OB_DUAL_BOOT_ENABLE) {
AdvOBInit.BootConfig &= (~OB_DUAL_BOOT_ENABLE);
} else {
AdvOBInit.BootConfig |= OB_DUAL_BOOT_ENABLE;
}
if (HAL_FLASHEx_AdvOBProgram(&AdvOBInit) != HAL_OK)
{
Error_Handler();
}
if (HAL_FLASHEx_OBProgram(&OBInit) != HAL_OK) {
Error_Handler();
}
if (HAL_FLASH_OB_Launch() != HAL_OK) {
Error_Handler();
}
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
}
2025-02-12 1:38 AM
Hello @melfice,
Make sure that the system memory is remapped correctly by setting the SYSCFG->MEMRMP register,
As noted in AN2606 " On devices with dual bank boot, to jump to system memory from user code the user must
first remap the system memory bootloader at address 0x00000000 using SYSCFG register
(except for STM32F7 series), then jump to bootloader"
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-02-19 10:55 PM
For records, I have managed to implement the dual bank code.
{
FLASH_OBProgramInitTypeDef OBInit;
FLASH_AdvOBProgramInitTypeDef AdvOBInit;
HAL_FLASH_Unlock();
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPERR);
HAL_FLASH_OB_Unlock();
HAL_FLASHEx_OBGetConfig(&OBInit);
OBInit.OptionType = OPTIONBYTE_USER;
HAL_FLASHEx_AdvOBGetConfig(&AdvOBInit);
AdvOBInit.OptionType = OPTIONBYTE_BOOTCONFIG;
if ((AdvOBInit.BootConfig &OB_DUAL_BOOT_ENABLE)==OB_DUAL_BOOT_ENABLE) {
AdvOBInit.BootConfig &= (~OB_DUAL_BOOT_ENABLE);
} else {
AdvOBInit.BootConfig |= OB_DUAL_BOOT_ENABLE;
}
if (HAL_FLASHEx_AdvOBProgram(&AdvOBInit) != HAL_OK)
{
Error_Handler();
}
if (HAL_FLASHEx_OBProgram(&OBInit) != HAL_OK) {
Error_Handler();
}
if (HAL_FLASH_OB_Launch() != HAL_OK) {
Error_Handler();
}
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.