STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hard Fault, after HAL_UART_Receive_DMA() is called.

Posted on September 28, 2017 at 08:43Hello!I am trying to use USART2 + DMA for Rx/Tx. Tx is working OK already.For Rx, I would like to use DMA circular mode.I use followings.  STM32L476 nucleo  STM32CubeMX, STM32CubeL4 1.9.0.After do workaround PLLM...

0690X00000608PcQAI.png 0690X00000608PhQAI.png 0690X00000608MUQAY.png 0690X00000608PmQAI.png

HAL I2C Interrupt code does not work on STM32F072

Posted on October 09, 2017 at 19:27I have been trying to get this to work for a few days now, read over several topics here and nothing I have tried has worked... I tried all the suggestions here as wellhttps://community.st.com/0D50X00009XkXWwSAN no...

STM32F767NI CAN RECEIVER PROBLEM

Posted on October 09, 2017 at 13:40I generate Can code from Cube MX. But i can't receive any data. i just want to receive data on CAN Receiver of STM32F767NI.I try to communicate via PCAN View. When i send data from PCAN-View the program said 'Bus-O...

Newbie + STM32L152C Discovery + USB DFU STM32CUBEMX

Posted on October 07, 2017 at 04:50I have the STM32L152C discovery board.  I used stm32cubemx to create a very simple bare bones project which will essentially allow me to try out the DFU mode with the PA11 and PA12 pins and a usb cable.  I am not g...

Change SPI baud rate on the fly: issue with DMA

Posted on October 09, 2017 at 11:04Hi,I am using SPI1 peripheral as master at 16 MHz on STM32L443, I can send and receive data correctly using DMA.My application requires to speed down SPI to 1MHz during a moment so I changed SPI baud rate on the fl...

creating screens for the STM32L053 Discovery Board

Posted on October 07, 2017 at 07:41Is there a utility program available that enables one to create custom screens for the STM32L053 Discover Board? I've looked at a couple of demo programs for the E-Paper display and see that the graphics elements a...

STM32F4xx + UART1 DMA + UART2

Posted on August 04, 2017 at 15:16hi,i have STM32F401 with uart1 configurate in DMA and i would like to add uart2 (in DMA or not)is it possible to do it?how i manage the IT flag?UART1 DMA, call fct :void HAL_UART_TxCpltCallback(UART_HandleTypeDef *U...

How can I send more than 3 CAN messages in a row...

Posted on December 26, 2016 at 10:31 Hi all; I try to send by CAN bus to 4 individual motor controllers their pwm speed settings in one go. I found out however, that the first three messages go through perfectly, but the forth message got stuck. ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.