2017-10-09 4:40 AM
I generate Can code from Cube MX. But i can't receive any data.
i just want to receive data on CAN Receiver of STM32F767NI.
I try to communicate via PCAN View. When i send data from PCAN-View the program said 'Bus-Off'. And receive interrupt never triggered.
APB1 periph clocks : 54Mhz
My configurations is here:
# Main Function
int main(void)
{ HAL_Init(); SystemClock_Config(); MX_GPIO_Init(); MX_ADC2_Init(); MX_ADC3_Init(); MX_CAN1_Init(); MX_CRC_Init(); MX_I2C2_Init(); MX_SDMMC1_SD_Init(); MX_SPI1_Init(); MX_TIM5_Init(); MX_TIM12_Init(); MX_UART4_Init(); MX_USART1_UART_Init(); MX_USART2_UART_Init(); MX_USART3_UART_Init(); MX_USART6_UART_Init(); MX_FATFS_Init(); MX_LWIP_Init(); MX_USB_DEVICE_Init(); if (HAL_CAN_Receive_IT(&hcan1, CAN_FIFO0) != HAL_OK) { /* Reception Error */ Error_Handler(); }while (1);
}
# CAN Init Function
static void MX_CAN1_Init(void)
{ static CanTxMsgTypeDef TxMessage; static CanRxMsgTypeDef RxMessage; hcan1.Instance = CAN1; hcan1.pTxMsg = &TxMessage; hcan1.pRxMsg = &RxMessage;hcan1.Init.TTCM = DISABLE;
hcan1.Init.ABOM = ENABLE; hcan1.Init.AWUM = DISABLE; hcan1.Init.NART = DISABLE; hcan1.Init.RFLM = DISABLE; hcan1.Init.TXFP = DISABLE; hcan1.Init.Mode = CAN_MODE_NORMAL; hcan1.Init.SJW = CAN_SJW_1TQ; hcan1.Init.BS1 = CAN_BS1_6TQ; hcan1.Init.BS2 = CAN_BS2_7TQ; hcan1.Init.Prescaler = 4;if (HAL_CAN_Init(&hcan1) != HAL_OK)
{ /* Initialization Error */ Error_Handler(); }}
# MSP Init Functions
void HAL_CAN_MspInit(CAN_HandleTypeDef* hcan)
{GPIO_InitTypeDef GPIO_InitStruct;
f(hcan->Instance==CAN1) { __HAL_RCC_CAN1_CLK_ENABLE(); GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_11; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF9_CAN1; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); HAL_NVIC_SetPriority(CAN1_RX0_IRQn, 0, 0); HAL_NVIC_EnableIRQ(CAN1_RX0_IRQn); HAL_NVIC_SetPriority(CAN1_RX1_IRQn, 0, 0); HAL_NVIC_EnableIRQ(CAN1_RX1_IRQn); }}
void HAL_CAN_MspDeInit(CAN_HandleTypeDef* hcan)
{if(hcan->Instance==CAN1)
{ __HAL_RCC_CAN1_CLK_DISABLE();HAL_GPIO_DeInit(GPIOA, GPIO_PIN_12|GPIO_PIN_11);
HAL_NVIC_DisableIRQ(CAN1_RX0_IRQn); HAL_NVIC_DisableIRQ(CAN1_RX1_IRQn);
}
}
2017-10-09 5:28 AM
I don't know about the PCAN View, and whether it shows that a node acknowledged a message.
You might need to recheck the CAN timing parameters for your application.
But, I see 2 things in your code:
1) you must configure the filters to enable reception. Otherwise no message will go into the FIFOs. (below config will catch any message and pipe it into FIFO0)
sFilterConfig.FilterNumber = 0;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig.FilterIdHigh = 0x0000;
sFilterConfig.FilterIdLow = 0x0000;
sFilterConfig.FilterMaskIdHigh = 0x0000;
sFilterConfig.FilterMaskIdLow = 0x0000;
sFilterConfig.FilterFIFOAssignment = 0;
sFilterConfig.FilterActivation = ENABLE;
sFilterConfig.BankNumber = 14;
if (HAL_CAN_ConfigFilter(&CanHandle, &sFilterConfig) != HAL_OK)
{
/* Filter configuration Error */
Error_Handler();
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
2) Since you are doing it interrupt based, you need to define the callback for CAN messages.
void HAL_CAN_RxCpltCallback(CAN_HandleTypeDef *CanHandle)
{
}�?�?�?
2017-10-09 8:45 AM
Thank you for reply,
i add filter and Callback function. The code with last changes:
static void MX_CAN1_Init(void)
{
CAN_FilterConfTypeDef sFilterConfig; static CanTxMsgTypeDef TxMessage; static CanRxMsgTypeDef RxMessage; hcan1.Instance = CAN1; hcan1.pTxMsg = &TxMessage; hcan1.pRxMsg = &RxMessage;hcan1.Init.TTCM = DISABLE;
hcan1.Init.ABOM = ENABLE; hcan1.Init.AWUM = ENABLE; hcan1.Init.NART = DISABLE; hcan1.Init.RFLM = DISABLE; hcan1.Init.TXFP = DISABLE; hcan1.Init.Mode = CAN_MODE_NORMAL; hcan1.Init.SJW = CAN_SJW_1TQ; hcan1.Init.BS1 = CAN_BS1_6TQ; hcan1.Init.BS2 = CAN_BS2_7TQ; hcan1.Init.Prescaler = 4;if (HAL_CAN_Init(&hcan1) != HAL_OK)
{ /* Initialization Error */ Error_Handler(); } sFilterConfig.FilterNumber = 0; sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK; sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT; sFilterConfig.FilterIdHigh = 0x0000; sFilterConfig.FilterIdLow = 0x0000; sFilterConfig.FilterMaskIdHigh = 0x0000; sFilterConfig.FilterMaskIdLow = 0x0000; sFilterConfig.FilterFIFOAssignment = 0; sFilterConfig.FilterActivation = ENABLE; sFilterConfig.BankNumber = 14;if (HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig) != HAL_OK)
{ /* Filter configuration Error */ Error_Handler(); } hcan1.pTxMsg->StdId = 0x321; hcan1.pTxMsg->ExtId = 0x01; hcan1.pTxMsg->RTR = CAN_RTR_DATA; hcan1.pTxMsg->IDE = CAN_ID_STD; hcan1.pTxMsg->DLC = 2;}And callback function:
void HAL_CAN_RxCpltCallback(CAN_HandleTypeDef *hcan1)
{if ((hcan1->pRxMsg->StdId == 0x321) && (hcan1->pRxMsg->IDE == CAN_ID_STD) && (hcan1->pRxMsg->DLC == 2))
{}
}
2017-10-09 8:48 AM
Hello Suat Berkant Gulen,
Let me also provide you some feedback.
First of all thanks Tiago for you answer. Definitely I agree that CAN filtering has to be configured and enabled. By default it is not done and I confirm that in such conditions it is not possible for STM32 to receive any CAN messages. By filling in all filter parameters with zeros and by callingHAL_CAN_ConfigFilter function you will enable CAN filtering in a way, that all CAN messages will be accepted.
Some time ago I created a presentation, which shows how to develop very simple CAN application for STM32F7 step by step. Please find attached both presentation and application. I hope it will be helpful to you.
Best regards
Szymon ________________ Attachments : STM32 F7 CAN.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyOD&d=%2Fa%2F0X0000000b6w%2F4gZLcGNtakiDMEcocCkZOXSAeS8TWG56mRn.1xng7Uo&asPdf=falseCAN_example.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyO3&d=%2Fa%2F0X0000000b6u%2FSwLz8hWcxLp7bITHwWFRqqkXPFrRbObEM0EB2pcxV2w&asPdf=false2017-10-09 10:40 AM
Thank you again and again.. It works. And thanks for help Tiago..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.