STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Issue with RTC maximum time resolution

Posted on September 19, 2017 at 16:51Hi,I'm using Nucleo STM32L476RG board and I have issue using specific configuration of RTC peripheral.Our embedded software requires precise timing for real time application.RTC is clocked by 32.768 kHz LSE and i...

Documentation issues in RM0316 rev 8

Posted on October 09, 2017 at 15:37Hello everyone,I've been reading the RM0316 Reference manual for STM32F303xB/C/D/E, STM32F303x6/8, STM32F328x8,STM32F358xC, STM32F398xE advanced ARM � -based MCUs, DocID022558 Rev 8 and have noticed following issue...

STM32F407 Start application from Bootloader

Posted on October 06, 2017 at 13:00Hi.     I have a STM32F407 application, developed with standard libraries which is launched by a bootloader. The application is loaded at flash address 0x08020000, the bootloader, once recognized a valid applicatio...

raffin by Associate III
  • 1368 Views
  • 2 replies
  • 0 kudos

Resolved! How to use DMA on STM32L0 with FIFO threshold ?

Posted on October 10, 2017 at 11:31Hello,I saw on the STM32L0 User Manual that FIFO mode and its threshold can be configured thanks to HAL_DMA_Init().For a given stream, HAL_DMA_Init() API allows programming the required configurationthrough the fol...

Resolved! NUCLEO32+STM32L011K4+MXCUBE Debug Issues

Posted on September 25, 2017 at 12:41Hi guys!I'm a completely newbie to the STM32 and to make some experiments I've bought a nucleo 32 board based on the STM32L011K4 microcontroller.Then I've downloaded and installed the Atollic TRUEStudio, the STCu...

CUBEMX STM32F103 GPIO REMAP

Posted on October 10, 2017 at 06:44#define __HAL_AFIO_REMAP_TIM2_PARTIAL_1() do{ CLEAR_BIT(AFIO->MAPR, AFIO_MAPR_TIM2_REMAP); \ SET_BIT(AFIO->MAPR, AFIO_MAPR_TIM2_REMAP_PARTIALREMAP1); \ }while(0U)CUBEMX version4.22.1used stm32f103vct6Sw debug mode ...

For External clock of STM32CubeMX

Posted on October 10, 2017 at 06:02English newbie, sorry.MCU:STM32F765IITx LQFP176tool:STM32CubeMXAbove by Pinout.If you want to enable external clock. High Speed Clock (HSE) BYPASS the Clock Source.And not only for the input pin, Output pin also do...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.