2017-10-09 2:42 AM
Hello,
for all families beside F1, the cubemx/mcu/IP/GPIO-STM32Xxxx_gpio_v1_0_Modes.xml give a complete list of the available device functions on a pin. For F1 files, only functions available on a pin that may get remapped are listed.
E.g. for F107 pin PA0, the available function 'ETH_CRS' is only listed in cubemx/mcu/STM32F107XXXx.xml, while mcu/IP/GPIO-STM32F107_gpio_v1_0_Modes.xml does not list it.
Having all information (pin name, pin function, remap value (no remap., 0..4) comes handy when generating support files from the XML headers.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.