STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucelo STM32F429ZI with 8742A PHY

Posted on October 10, 2017 at 22:34Hi,I am using the latest ST32CubeMx Ver. 4.22.Creating a new project with the wizard and selecting my target board Nucelo STM32F429ZI.When selecting the middleware ETH connectivity I have DP8348 as only choice wher...

STM32L071 DMA from Mem to Peri

Posted on October 11, 2017 at 14:33Hi,I want to use DMA for transfer data from memory (uint16_t DMA_BUFF[10]) to register TM21.ARR. I want to use TIM6 for generating events every 50 ms for DMA to transfer DMA_BUFF[xx] to TIM21.ARR.In First 50 ms I w...

JAN R by Associate III
  • 1850 Views
  • 5 replies
  • 0 kudos

Hard Fault with ''STemWin_HelloWorld'' Example.

Posted on October 11, 2017 at 04:05Compiler:           IAR Workbench v8.11.3Graphics:           STemWinHardware:          STM32746G Discovery BoardHAL Version:     V1.8.0Demo Project:   C:\STM32Cube_FW_F7_V1.8.0\Projects\STM32746G-Discovery\Applicat...

ç�?¨STM32F765芯片外部能扩展2片8ä½�å�•颗256Mbçš„SDRAMå�—,怎么连接呢?

Posted on October 11, 2017 at 10:28请问ç�?¨STM32F765芯片外部能扩展2片8ä½�å�•颗256Mbçš„SDRAMå�—,怎么连接呢?

1 1 by Associate
  • 728 Views
  • 0 replies
  • 0 kudos

NUCLEO-F401RE not connecting to PC

Posted on October 11, 2017 at 10:14I just got a NUCLEO-F401RE board along with the NUCLEO-53L0A1 proximity sensors board, When I connect it to the lap, it is not recognized as a USB drive. Anybody seen this and any resolution please.#nucleo-f401re

stm32f429 TIM10_input_capture mode question

Posted on October 10, 2017 at 14:14setting CC1IE:1 (TIM10->DIER) capture is good, but not occur capture interruptwhy?this is my sorce code  volatile uint32_t temp2 =0;  /*******GPIOG_Ouput_Init****************/  //RCC  RCC->AHB1ENR |= 0x00000001<<6;...

STM32F7 FMC Synchronous CLKDIV=3

Posted on October 10, 2017 at 17:24I'm looking to use the FMC in Synchronous PSRAM 16-bit mode, and need to run CLKDIV of 3 (or 4).  The reference manual (RM0410) waveforms seem to show only a setting of CLKDIV=2.  In figure 50/51, CLK is shown togg...

more than one chanel ADC in STM32F030

Posted on October 11, 2017 at 00:03Hi, i have a problem with to program multiple ADCs Conversions. normally to program a single channel (0,1,2,3....n) MX_ADC_Init();HAL_ADC_Start(&hadc);adcValue=HAL_ADC_GetValue(&hadc);how do i read more than one AD...

How to find project specific files in CubeMx?

Posted on October 10, 2017 at 18:50A Cube template, example or whatever contains around 150 files. I don't think that each of them is edited for every project but some of course are. When trying to use those examples the user should know what files ...

LMI2 by Lead
  • 1930 Views
  • 4 replies
  • 0 kudos

STM32F407 debuugger not working when PORTA in use

Posted on October 10, 2017 at 12:42Hi.Using a STM32F407 I am having an issue using the debugger when PORTA is in use. The debugger works fine when PORTA is not in use. I am using MCO1 which is on PORTA and when I set the MODER register the debugger ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.