2017-10-10 5:14 AM
setting CC1IE:1 (TIM10->DIER)
capture is good, but not occur capture interrupt
why?
this is my sorce code
volatile uint32_t temp2 =0;
/*******GPIOG_Ouput_Init****************/ //RCC RCC->AHB1ENR |= 0x00000001<<6; //GPIOG CLK EN //GPIOG GPIOG->MODER |= 0x00000001<<(2*14);//01:output mode (PORT14) GPIOG->PUPDR |= 0x00000000; //00:no-pull_up, no-pull_down GPIOG->OTYPER |= 0x00000000; //0:PUSH-PULL GPIOG->OSPEEDR|= 0x00000000; //00:Low Speed /*******TIM10_InputCapture Init*********/ //NVIC NVIC->ISPR[0] |= 0x00000001<<25; //TIM10 position 25 //RCC RCC->AHB1ENR |= 0x00000001<<5; //GPIOF CLK EN temp2 = 0; RCC->APB2ENR |= 0x00000001<<17; //TIM10 CLK EN //GPIOF AF GPIOF->MODER |= 0x00000002<<(2*6); //PF6 10: AF MODE GPIOF->OTYPER |= 0x00000000; //0:PUSH-PULL GPIOF->OSPEEDR|= 0x00000000; //00:Low Speed GPIOF->PUPDR |= 0x00000000; //:no PU, no PD GPIOF->AFR[0] |= 0x00000003<<(4*6); //0011:AF3(TIM10) //TIM10 TIM10->CCMR1 |= 0x00000001; //CC1S: 01(configured as Input) TIM10->CCMR1 |= 0x00000008; //IC1PSC: 10(capture is done once every 4 events) TIM10->CCER |= 0x0000000A; //CC1P: 1, CC1NP: 1 (11: both edges) TIM10->CCER |= 0x00000001; //CC1E: 1(Capture EN) TIM10->DIER |= 0x00000002; //CC1IE:1(CC1 interrupt EN) TIM10->PSC = 15999; //Prescaler 16MHz/(15999 + 1) = 1clk = 1ms TIM10->ARR = 9999; // 1ms * (9999+1), overflow is 10 sec TIM10->CR1 |= 0x00000001; //CEN: 1(counter EN) temp2 = 1; /* USER CODE END 2 */.
.
/* USER CODE BEGIN 4 */
void TIM1_UP_TIM10_IRQHandler(void){ /* USER CODE BEGIN TIM1_UP_TIM10_IRQn 0 */ HAL_GPIO_TogglePin(GPIOG,GPIO_PIN_14); /* USER CODE END TIM1_UP_TIM10_IRQn 0 */ //HAL_TIM_IRQHandler(&htim10); TIM10->SR &= 0xFFFFFFFD; //CC1F : 0 reset /* USER CODE BEGIN TIM1_UP_TIM10_IRQn 1 *//* USER CODE END TIM1_UP_TIM10_IRQn 1 */
}/* USER CODE END 4 */2017-10-10 5:42 AM
TIM1_UP_TIM10_IRQHandler
As its name says, this is the handler for update interrupt, not the capture-compare interrupts - TIM1 has several separate interrupt vectors.
You want to use TIM1_CC_IRQHandler().
JW
2017-10-10 11:15 PM
Sorry, I've overlooked that it's TIM10 not TIM1...
Good catch. I tend to use the CMSIS functions for NVIC register manipulation (NVIC_SetPriority(), NVIC_EnableIRQ(), etc.) together with the xxxx_IRQn symbols.
JW
2017-10-10 11:51 PM
Thank you
My misstake is NVIC->ISPR[0] = 0x00000001<<25;
I should have used ISER, but I used ISPR.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.