2017-11-21 6:17 PM
I am trying to configure I2S3 in Fullduplex Master RX mode, 48KHz sample rate. Hal Configuration is as shown below
hAudioFDI2s
.
Init
.
AudioFreq
=
AudioFreq
;
hAudioFDI2s
.
Init
.
ClockSource
=
I2S_CLOCK_PLL
;
hAudioFDI2s
.
Init
.
CPOL
=
I2S_CPOL_LOW
;
hAudioFDI2s
.
Init
.
DataFormat
=
I2S_DATAFORMAT_16B
;
hAudioFDI2s
.
Init
.
MCLKOutput
=
I2S_MCLKOUTPUT_DISABLE
;
hAudioFDI2s
.
Init
.
Mode
=
I2S_MODE_MASTER_RX
;
hAudioFDI2s
.
Init
.
Standard
=
I2S_STANDARD
;
hAudioFDI2s
.
Init
.
FullDuplexMode
=
I2S_FULLDUPLEXMODE_ENABLE
;
I2S PLLs are configured successfully for 48KHz sample rate, I confirmed it by probing the WS and BCLK pins
WS: 48KHz
Bit Clock: 3.072Mhz ( 48 * 16bit * 2ch*)*2 (for extended mode) = 3.072KHz, and I have connected this to an external codec configured to receive I2S signals from ST.
However, the problem I am facing is I get distorted audio in only left channel. And above setup works well with the 16KHz no distortion in both channels. I confirmed the same behavior with different codec too. So, I don't think this is a misconfiguration in codec.
I am using DMA to transmit data over I2S
hdma_i2sRx
.
Init
.
Channel
=
DMA_CHANNEL_0;hdma_i2sRx
.
Init
.
Direction
=
DMA_PERIPH_TO_MEMORY
;
hdma_i2sRx
.
Init
.
PeriphInc
=
DMA_PINC_DISABLE
;
hdma_i2sRx
.
Init
.
MemInc
=
DMA_MINC_ENABLE
;
hdma_i2sRx
.
Init
.
PeriphDataAlignment
=
DMA_PDATAALIGN_HALFWORD
;hdma_i2sRx
.
Init
.
MemDataAlignment
=
DMA_MDATAALIGN_HALFWORD
;
hdma_i2sRx
.
Init
.
Mode
=
DMA_NORMAL
;
hdma_i2sRx
.
Init
.
Priority
=
DMA_PRIORITY_HIGH
;
hdma_i2sRx
.
Init
.
FIFOMode
=
DMA_FIFOMODE_ENABLE
;
hdma_i2sRx
.
Init
.
FIFOThreshold
=
DMA_FIFO_THRESHOLD_FULL
;
hdma_i2sRx
.
Init
.
MemBurst
=
DMA_MBURST_SINGLE
;
hdma_i2sRx
.
Init
.
PeriphBurst
=
DMA_PBURST_SINGLE
;
hdma_i2sRx
.
Instance
= DMA1_Stream0
Tx configuration:
hdma_i2s_ext_tx
.
Init
.
Channel
= DMA_CHANNEL_2
;
hdma_i2s_ext_tx
.
Init
.
Direction
=
DMA_MEMORY_TO_PERIPH
;
hdma_i2s_ext_tx
.
Init
.
PeriphInc
=
DMA_PINC_DISABLE
;
hdma_i2s_ext_tx
.
Init
.
MemInc
=
DMA_MINC_ENABLE
;
hdma_i2s_ext_tx
.
Init
.
PeriphDataAlignment
=
DMA_PDATAALIGN_HALFWORD
;hdma_i2s_ext_tx
.
Init
.
MemDataAlignment
=
DMA_MDATAALIGN_HALFWORD
;
hdma_i2s_ext_tx
.
Init
.
Mode
=
DMA_NORMAL
;
hdma_i2s_ext_tx
.
Init
.
Priority
=
DMA_PRIORITY_HIGH
;
hdma_i2s_ext_tx
.
Init
.
FIFOMode
=
DMA_FIFOMODE_ENABLE
;
hdma_i2s_ext_tx
.
Init
.
FIFOThreshold
=
DMA_FIFO_THRESHOLD_FULL
;
hdma_i2s_ext_tx
.
Init
.
MemBurst
=
DMA_MBURST_SINGLE
;
hdma_i2s_ext_tx
.
Init
.
PeriphBurst
=
DMA_PBURST_SINGLE
;
hdma_i2s_ext_tx
.
Instance
=
DMA1_Stream5
;I was wondering is there any known issues with the I2S3 in extended mode? or Am I configuring it wrongly?
Thank you,
Raj
#i2s-dma-audio #i2s-i2s2ext2017-11-22 1:44 AM
However, the problem I am facing is I get distorted audio in only left channel.
What exactly do you mean by distorted audio?
I2S contains data for both channels in one stream of data, one data pin, and DMA is channel-agnostic, so it's quite unlikely the problem is here. Can't it be your primary data source? As an experiment, fill a buffer with a simple pattern - a square wave, or a simple triangle - and play it back repeatedly - does the problem still persist?
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.